Products
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
Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
PicoZed SDR Software-Defined Radio About U-Boot for picozed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 964 views
  • Users 0 members are here
Related

About U-Boot for picozed

e14 Contributor
e14 Contributor over 10 years ago

Hi  all,

       I have a DVSK board(Picozed, QSPI+eMMC ). And download u-boot-xlnx-xilinux-v2015.4, using different config to build uboot, It's get different result.

       1)make zynq_picozed_defconfig to build uboot, and create boot image, download to QSPI flash. The uboot can recognize the eMMC flash and cannot using sf command.  The detail info:

       U-Boot 2015.07 (Jun 20 2016 - 13:55:28 +0800)

 
Model: Zynq PicoZed Board
DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
Using default environment
 
In:    serial
Out:   serial
Err:   serial
Model: Zynq PicoZed Board
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Copying Linux from QSPI flash to RAM...
Unknown command 'sf' - try 'help'
zynq-uboot> mmcinfo
Device: zynq_sdhci
Manufacturer ID: fe
OEM: 14e
Name: MMC04
Tran Speed: 52000000
Rd Block Len: 512
MMC version 4.4.1
High Capacity: Yes
Capacity: 3.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 KiB
HC WP Group Size: 4 MiB
User Capacity: 3.5 GiB
Boot Capacity: 16 MiB ENH
RPMB Capacity: 128 KiB ENH
zynq-uboot>              

       2)make zynq_zed_defconfig to build uboot, The uboot can recognize the SPI flash and cannot using mmcinfo command.  The detail info:

U-Boot 2015.07 (Jun 20 2016 - 13:53:03 +0800)
 
Model: Zynq Zed Development Board
DRAM:  ECC disabled 512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
*** Warning - bad CRC, using default environment
 
In:    serial
Out:   serial
Err:   serial
Model: Zynq Zed Development Board
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Copying Linux from QSPI flash to RAM...
SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
device 0 offset 0x100000, size 0x500000
SF: 5242880 bytes @ 0x100000 Read: OK
device 0 offset 0x600000, size 0x20000
SF: 131072 bytes @ 0x600000 Read: OK
Copying ramdisk...
device 0 offset 0x620000, size 0x5e0000
SF: 6160384 bytes @ 0x620000 Read: OK
Wrong Image Format for bootm command
ERROR: can't get kernel image!
zynq-uboot> mmcinfo
sdhci_set_clock: Internal clock never stabilised.
 
And I want to know  how to config to recognize the QSPI and eMMC in uboot?  
 
 Thanks a lot.
  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi gomo,

    If you look under the hood for PetaLinux, when SPI+eMMC boot mode is set within the project configuration the following config options are set:

    #define CONFIG_ZYNQ_SDHCI1t0xE0101000
    #define CONFIG_ZYNQ_QSPI

    Also, the following configuration options become removed:

    #define CONFIG_ZYNQ_SDHCI0t0xE0100000

    You will also need to setup appropriate U-Boot ENV macros to boot from QSPI+eMMC but the details of those can vary based upon how your Linux is being configured.  PetaLinux is a good example of how to do some of these different boot options because you can change things within the config menu and then go back and see which pieces of source code were modified to accommodate the changes.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi,

    Did you manage to solve this trouble ?

    I'm quite in the same situation (all but xilinx-v2015.3 version of U-boot). I compared with the U-boot version in PetaLinux 2015.04 but without success.

    The only error that appears at boot time is

       SF: Detected S25FL128S_64K with page size 256 Bytes, erase size 64 KiB, total 16 MiB
       *** Warning - bad CRC, using default environment

    As soon as I enter "mmcinfo" command (did not try another), U-boot stops/hangs with the following message (when it appears) :

       my-zynq> mmcinfo
       sdhci_set_clock: Internal clock never stabilised.

    Something is not correctly set but I cannot find what ? Any help would be appreciated.

    Many thank in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi,

    I came to the Xilinx-v2016.2 version of U-boot and the situation evolved a bit, but some troubles remain :

    1. the QSPI flash is still not detected. When U-boot starts, the following error message still appears :

    Invalid bus 0 (err=-19)
    *** Warning - spi_flash_probe() failed, using default environment

    Any attempt to access the QSPI flash (sf probe) failed with the same error message.

    Here is the QSPI description in the device tree :

                    qspi: spi@e000d000 {
                            clock-names = "ref_clk", "pclk";
                            clocks = <&clkc 10>, <&clkc 43>;
                            compatible = "xlnx,zynq-qspi-1.0";
                            interrupt-parent = <&intc>;
                            interrupts = <0 19 4>;
                            reg = <0xe000d000 0x1000>;
                            #address-cells = <1>;
                            #size-cells = <0>;
                            is-dual = <0x0>;
                            num-cs = <0x1>;
                            xlnx,fb-clk = <0x0>;
                            xlnx,qspi-mode = <0x0>;
    
                            flash@0 {
                                    compatible = "micron,s25fl129p1";
                                    reg = <0x0>;
                                    #address-cells = <0x1>;
                                    #size-cells = <0x1>;
                                    spi-max-frequency = <50000000>;
    
                                    partition@0x00000000 {
                                            label = "boot";
                                            reg = <0x0 0x500000>;
                                    };
    
                                    partition@0x00500000 {
                                            label = "bootenv";
                                            reg = <0x500000 0x20000>;
                                    };
    
                                    partition@0x00520000 {
                                            label = "kernel";
                                            reg = <0x520000 0xa80000>;
                                    };
    
                                    partition@0x00fa0000 {
                                            label = "spare";
                                            reg = <0xfa0000 0x0>;
                                    };
                            };
                    };
    

    What's wrong ?

    2.  The eMMC is now viewed :

    Zynq> mmcinfo
    Device: sdhci@e0101000
    Manufacturer ID: fe
    OEM: 14e
    Name: MMC04
    Tran Speed: 52000000
    Rd Block Len: 512
    MMC version 4.4.1
    High Capacity: Yes
    Capacity: 3.5 GiB
    Bus Width: 4-bit
    Erase Group Size: 512 KiB
    HC WP Group Size: 4 MiB
    User Capacity: 3.5 GiB
    Boot Capacity: 16 MiB ENH
    RPMB Capacity: 128 KiB ENH

    But for unknown reason, I cannot read the partition table :

    Zynq> mmc dev 0
    switch to partitions #0, OK
    mmc0(part 0) is current device
    Zynq> mmc part
    ## Unknown partition table

    What could be wrong again ?

     

    Any help about those points would be appreciated. Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Hi,

    Did you manage to solve this trouble ?  I am in the same situation with picozed.

       Copying Linux from QSPI flash to RAM...

        Unknown command 'sf' - try 'help'
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • totowkaee
    0 totowkaee over 7 years ago

    Hi,

    i had same problem and here is how i fixed it:

    in <your_board>_defconfig file add

    CONFIG_CMD_SF=y

    CONFIG_ZYNQ_QSPI=y

    and i also added the followong lines, but i am not sure if we really need all of them:

    CONFIG_SPI_FLASH=y

    CONFIG_SPI_FLASH_BAR=y

    CONFIG_SPI_FLASH_MACRONIX=y

    CONFIG_SPI_FLASH_SPANSION=y

    CONFIG_SPI_FLASH_STMICRO=y

    CONFIG_SPI_FLASH_WINBOND=y

    Hopefully this will work for others...