Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RFSoC Boards RFSoC rftool console command argument.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 2534 views
  • Users 0 members are here
Related

RFSoC rftool console command argument.

khabnl
khabnl over 4 years ago

Hello,

 I am attempting to load the “RF_Init.cfg”  file manually using “rftool” console command.

The ZCU208 Linux boot-up automatically loads the “/mnt/hdlcoder_rd/RF_Init.cfg” file and initializes it.

 If I delete the “/mnt/hdlcoder_rd/RF_Init.cfg” file then the console shows an error message.

rf_init: Could not locate /mnt/hdlcoder_rd/RF_Init.cfg ! Exiting...

 

Does anyone know what rftool options are for loading user configuration files at the console?

zynqrf> rftool

Version number; 2.4


Board version ZCU208


RFCLK v1.4

RFCLK v1.4 Init Done
starting server...
starting data server...
IP Address of the board: 192.168.1.101
Server Init Done

 Thanks,

  • Sign in to reply
  • Cancel

Top Replies

  • mbrown
    mbrown over 4 years ago +2 verified
    From the linux terminal prompt you can issue the following command to reload RF_Init.cfg zynqrf> mw-rf-init
  • lightcollector
    lightcollector over 4 years ago in reply to khabnl +1
    Hi, Just curious why you would need to reload the settings again? The commands in RF_Init.cfg are executed when the board powers up. Are you looking for a way to change NCO / Mixer frequencies? If so and…
  • mbrown
    +1 mbrown over 4 years ago

    From the linux terminal prompt you can issue the following command to reload RF_Init.cfg

    zynqrf> mw-rf-init

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • khabnl
    0 khabnl over 4 years ago in reply to mbrown

    Hello @mbrown,

    Thank you. I confirmed mw-rf-init command, and it is working as a rftool TCP/IP client.

    I can reinitialize PLL and RFDC parameters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lightcollector
    0 lightcollector over 4 years ago in reply to khabnl

    Hi,  Just curious why you would need to reload the settings again?  The commands in RF_Init.cfg are executed when the board powers up.  Are you looking for a way to change NCO / Mixer frequencies?  If so and you are using Matlab you should consider using the following:  https://www.mathworks.com/help/supportpkg/xilinxsoc/ref/soc.rfdataconverter-system-object.html

    You are certainly welcome to use the mw-rf-init command but do keep in mind it is possible that in future releases this will change a bit.

    Good luck with your project!