Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
RFSoC Boards About status LEDs of RFSoC ZCU208 board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 1060 views
  • Users 0 members are here
Related

About status LEDs of RFSoC ZCU208 board

Hiroaki
Hiroaki over 2 years ago

Getting started with HDL Coder for the Xilinx ZCU208 RFSoC Gen 3 development board — hdlcoder-docs v1.0.0 documentation (rfsoc-hdlcoder.readthedocs.io)
Follow step8, I inserted SD card. But, LED of "DS2" turned on red in RFSoC ZCU208 board and it did not turn green over time. I think there is a problem with the operation of the FPGA, but I don't know the cause.

If anyone knows the cause or solution, please let me know.

  • Sign in to reply
  • Cancel

Top Replies

  • lightcollector
    lightcollector over 2 years ago +1
    Hi Hiroaki, I am not sure either, no one else has reported this issue and DS2 is not user controlled. I would check to make sure the SD card contents are not corrupted. Some kinds of SD cards sometimes…
Parents
  • mbrown
    0 mbrown over 2 years ago

    Adding to what lightcollector recommended, double-check that `system.bit` was successfully copied to the SD card. If it is missing, the FPGA has no bitstream to load.

    Also, confirming that DS2 is indeed the indicator for a successful boot of the FPGA/PL part of the device.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 2 years ago

    Adding to what lightcollector recommended, double-check that `system.bit` was successfully copied to the SD card. If it is missing, the FPGA has no bitstream to load.

    Also, confirming that DS2 is indeed the indicator for a successful boot of the FPGA/PL part of the device.