Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development baremetal programming on picozed 7015/7030 (v1)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 1905 views
  • Users 0 members are here
Related

baremetal programming on picozed 7015/7030 (v1)

openhacker
openhacker over 7 years ago

I'm following the tutorial in

Tutorial 2 -- First application - Hello world for Vivado 2016.4 (I got vivado 2016.4 so I can follow the tutorial verbatim)

 

It says:

8. Click Browse and select the System_wrapper.hdf file generated during the

Export process from Vivado. This will be included in the archive provided by the

hardware engineer. Or, if you are continuing from the first tutorial, you will find

it in a similar location as here:

C:\Avnet\MicroZed\Projects\MZ_Basic_System\MZ_Basic_System.sdk\

 

I didn't see (or know where to get) the "System_wrapper.hdf file.

 

So I got 2016.04 vivado.

I followed:

Tutorial 01 Build the Zynq Hardware Platform

for 2016.4

(since that's the newest one -- when I get something working, I'll move on to something newer)

 

On page 3, it lists a whole range of picozed boards from em.avnet.com.   I figured the process would be straightforward.

 

But attached is what I see (no picozed).

 

FWIW, I've been doing embedded work for 30 years ;-)   This is new for me (I have a client who wants me to do software work,

not hardware work).

 

I'm interested in getting my jtag adapter working -- but it seems I need a good "board description" to do anything.

 

marty

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • openhacker
    openhacker over 7 years ago in reply to jafoste4 +1
    I generally don't use windows if I don't have to. I used 2016.4 since the tutorials targeted that (and their screen shots of some of the buttons were backwards) -- but I didn't have to guess and wonder…
Parents
  • neuromodulator
    neuromodulator over 7 years ago

    I'm new to FPGAs and got a Digilent Cmod Spartan7, so I'm not sure how much of this applies to the Zenq. For my FPGA at least I had to download a file from Digilent to add the board support. Still that support apparently is only required to get some visual programming blocks, basically pin dependent stuff. As a matter of fact I've completely ignored the board selection (I'm just doing HDL at this point) and just selected the FPGA chip, and thats all I need to get it to work. Vivado requires to know what chip you are using because otherwise I doesn't know how to do logic synthesis, as it depends on the specific FPGA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neuromodulator
    neuromodulator over 7 years ago

    I'm new to FPGAs and got a Digilent Cmod Spartan7, so I'm not sure how much of this applies to the Zenq. For my FPGA at least I had to download a file from Digilent to add the board support. Still that support apparently is only required to get some visual programming blocks, basically pin dependent stuff. As a matter of fact I've completely ignored the board selection (I'm just doing HDL at this point) and just selected the FPGA chip, and thats all I need to get it to work. Vivado requires to know what chip you are using because otherwise I doesn't know how to do logic synthesis, as it depends on the specific FPGA.