Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development zedboard embedded linux version
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 364 subscribers
  • Views 3189 views
  • Users 0 members are here
Related

zedboard embedded linux version

e14 Contributor
e14 Contributor over 14 years ago

Hello,

some questions about the pre-installed linux:

1) Is this embedded linux version that from the linux-xlnx xilinx-git repository?

http://git.xilinx.com/?p=linux-xlnx.git;a=summary

2) Do you supply all sources, build scripts and project files, or do I have to struggle through the xilinx documentation to get it working for my own project?

- Or do you supply only the working binary of the linux-system?

3) Do you supply the planAhead and EDK Project Files for the zedboard?

Philipp

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I build and almost booted an ubuntu kernel on the zed according to following guidelines.
    http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq#fixing_issues_with_pulse_audio

    I passed FSBL, bitstream loading, uboot, zimage and device tree loading. But it gives the following error message when it is trying to the load the filesystem.

    Kernel panic: no init found. Try passing init= option to kernel.

    The device tree contains the following option for FS.
    bootargs = "console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0";


    What are the options for init?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello,

    Had anyone finally solved the kernel panic problem/s?

    It happens me the same, I'm trying to build my own embedded linux distro. using u-boot as a bootloader, digilent kernel (new kernel uploaded in their git, based on 3.6 kernel), *.dtb obtained with the script tools as xilinx "explain" in his wiki page (I kept bootargs like the out of box factory made) and Bootloader too, (I'll post something soon about my bootargs' discoveries), I use buildroot 2011.11.1 to compile the kernel and to build my root filesystem image with the basic libraries.

    Copying *.dtb, zImage, ramdisk.image.gz and BOOT.BIN to SD and powering up. When the filesystem begins to being mounted:

    >EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    >VFS: Mounted root (ext2 filesystem) on device 1:0.
    >Freeing init memory: 148K
    >Failed to execute /sbin/init.  Attempting defaults...
    >Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
    >CPU0: stopping

    And then it hangs. If I try my zImage with the other factory made files of the SD it works.

    Im trying different combinations of uClibc versions, binutil versions, and GCC versions inside buildroot, could somebody help me?

    If anybody need some more info or had any idea please answer or mail me, Im running out of ideas.

    Thanks for your time. Best regards,

    u00C1lvaro Bustos, Universidad Politu00E9cnica de Madrid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hello,

    Had anyone finally solved the kernel panic problem/s?

    It happens me the same, I'm trying to build my own embedded linux distro. using u-boot as a bootloader, digilent kernel (new kernel uploaded in their git, based on 3.6 kernel), *.dtb obtained with the script tools as xilinx "explain" in his wiki page (I kept bootargs like the out of box factory made) and Bootloader too, (I'll post something soon about my bootargs' discoveries), I use buildroot 2011.11.1 to compile the kernel and to build my root filesystem image with the basic libraries.

    Copying *.dtb, zImage, ramdisk.image.gz and BOOT.BIN to SD and powering up. When the filesystem begins to being mounted:

    >EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    >VFS: Mounted root (ext2 filesystem) on device 1:0.
    >Freeing init memory: 148K
    >Failed to execute /sbin/init.  Attempting defaults...
    >Kernel panic - not syncing: No init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
    >CPU0: stopping

    And then it hangs. If I try my zImage with the other factory made files of the SD it works.

    Im trying different combinations of uClibc versions, binutil versions, and GCC versions inside buildroot, could somebody help me?

    If anybody need some more info or had any idea please answer or mail me, Im running out of ideas.

    Thanks for your time. Best regards,

    u00C1lvaro Bustos, Universidad Politu00E9cnica de Madrid.