Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development zedboard embedded linux version
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 364 subscribers
  • Views 3176 views
  • Users 0 members are here
Related

zedboard embedded linux version

e14 Contributor
e14 Contributor over 14 years ago

Hello,

some questions about the pre-installed linux:

1) Is this embedded linux version that from the linux-xlnx xilinx-git repository?

http://git.xilinx.com/?p=linux-xlnx.git;a=summary

2) Do you supply all sources, build scripts and project files, or do I have to struggle through the xilinx documentation to get it working for my own project?

- Or do you supply only the working binary of the linux-system?

3) Do you supply the planAhead and EDK Project Files for the zedboard?

Philipp

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I build and almost booted an ubuntu kernel on the zed according to following guidelines.
    http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq#fixing_issues_with_pulse_audio

    I passed FSBL, bitstream loading, uboot, zimage and device tree loading. But it gives the following error message when it is trying to the load the filesystem.

    Kernel panic: no init found. Try passing init= option to kernel.

    The device tree contains the following option for FS.
    bootargs = "console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0";


    What are the options for init?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    hi,
    my command string says:
    console=ttyPS0,115200n8 earlyprintk rootfstype=ext4 root=/dev/mmcblk0p2 rw rootdelay=1 init=/sbin/init
    also i had to set the CONFIG_CMDLINE_FORCE parameter in order to avoid passing parameters to the kernel using u-boot.
    C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    hi,
    my command string says:
    console=ttyPS0,115200n8 earlyprintk rootfstype=ext4 root=/dev/mmcblk0p2 rw rootdelay=1 init=/sbin/init
    also i had to set the CONFIG_CMDLINE_FORCE parameter in order to avoid passing parameters to the kernel using u-boot.
    C.