Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq Base TRD 14.1 On Zedboard?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 595 views
  • Users 0 members are here
Related

Zynq Base TRD 14.1 On Zedboard?

e14 Contributor
e14 Contributor over 14 years ago


Has anyone had any luck getting the Xilinx Zynq Base TRD 14.1 running on the Zedboard?  I know it is intended for the ZC702 Evaluation Board, but I hoped the hardware would be similar enough to get close.

I tried just installing the binaries on the SD card and booting it, but it hung on:

INFO : Initialize HDMI OUT

The TRD is along the lines of a potential application, so I would like to see it run if it isn't impossible.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi.
    I made my ZYNQ board. It has DDR3 512MB. I used reference example "zynq_base_trd_14.2".
    I did boot linux kernel(v3.3) already but I had a problem with video driver(xylonfb).

    The video frame buffer's address is 0x30000000 ~ 0x37FFFFFF at ZC702 because it has DDR3 1GB.
    So I changed it "0x10000000 ~ 0x17FFFFFF" at DTS file, because my board has 512MB.

    DTS modification
    *********************************************
                    logicvc0: logicvc@40030000 {
                            compatible = "xylon,logicvc-2.05.b", "xylon,logicvc-2.05.c";
                            reg = <0x40030000 0x6000>;
                            interrupt-parent = <&gic>;
                            interrupts = < 0 59 0 >;
                            buffer-0-offset = <1080>;
                            buffer-1-offset = <1080>;
                            buffer-2-offset = <1080>;
                            buffer-3-offset = <1080>;
                            buffer-4-offset = <1080>;
                            ...............
                            use-xtreme-dsp = <2>;
                            vmem-baseaddr = <0x10000000>;
                            vmem-highaddr = <0x17ffffff>;
                            vmem-data-bus-width = <64>;
                            vmem-interface = <2>;
                    };
    *****************************************************

    But I've got ioremap error.
    *****************************************************
    ### reg_base_phys = 0x40030000,reg_base_virt = 0xef898000
    ### layer_data->fb_phys = 0x10000000, layer_data->fb_size = 0x1950000
    ### layer_data->xylonfb_cd->xylonfb_flags = 0x10, FB_DMA_BUFFER = 0x1
    ------------[ cut here ]------------
    WARNING: at arch/arm/mm/ioremap.c:241 __arm_ioremap_pfn_caller+0x108/0x1a4()
    Modules linked in:
    [<c0012928>] (unwind_backtrace+0x0/0xe0) from [<c001e84c>] (warn_slowpath_common+0x4c/0x64)
    [<c001e84c>] (warn_slowpath_common+0x4c/0x64) from [<c001e87c>] (warn_slowpath_null+0x18/0x1c)
    [<c001e87c>] (warn_slowpath_null+0x18/0x1c) from [<c001733c>] (__arm_ioremap_pfn_caller+0x108/0x1a4)
    [<c001733c>] (__arm_ioremap_pfn_caller+0x108/0x1a4) from [<c0017438>] (__arm_ioremap_caller+0x50/0x54)
    [<c0017438>] (__arm_ioremap_caller+0x50/0x54) from [<c01742bc>] (xylonfb_init_driver+0x3f4/0xaf0)
    [<c01742bc>] (xylonfb_init_driver+0x3f4/0xaf0) from [<c0175fdc>] (xylonfb_of_probe+0x71c/0x800)
    [<c0175fdc>] (xylonfb_of_probe+0x71c/0x800) from [<c019a6c8>] (platform_drv_probe+0x14/0x18)
    [<c019a6c8>] (platform_drv_probe+0x14/0x18) from [<c01997d0>] (driver_probe_device+0xc8/0x184)
    [<c01997d0>] (driver_probe_device+0xc8/0x184) from [<c01998ec>] (__driver_attach+0x60/0x84)
    [<c01998ec>] (__driver_attach+0x60/0x84) from [<c01983a0>] (bus_for_each_dev+0x48/0x74)
    [<c01983a0>] (bus_for_each_dev+0x48/0x74) from [<c01990ec>] (bus_add_driver+0x98/0x214)
    [<c01990ec>] (bus_add_driver+0x98/0x214) from [<c0199dc4>] (driver_register+0xa0/0x134)
    [<c0199dc4>] (driver_register+0xa0/0x134) from [<c041fab4>] (xylonfb_of_init+0x30/0x54)
    [<c041fab4>] (xylonfb_of_init+0x30/0x54) from [<c000858c>] (do_one_initcall+0x90/0x160)
    [<c000858c>] (do_one_initcall+0x90/0x160) from [<c040f854>] (kernel_init+0x84/0x128)
    [<c040f854>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
    ---[ end trace 39f178f86d67a36c ]---
    Error xylonfb ioremap REGS 0xEF898000 FB 0x0
    logicvc: probe of 40030000.logicvc failed with error -12
    ********************************************

    This error point is here.
    *********************************************
    linux_xlnx/drivers/video/xylon/xylonfb/core/xylonfb.c
    at 750 line

    753         } else {
    754                 pr_notice("###2 Video bufer ioremapping
    ");     // by cokang
    755                 layer_data->fb_virt =
    756                         ioremap_wc(layer_data->fb_phys, layer_data->fb_size);
    757         }
    *********************************************

    I don't know how to solve it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I met the same problem...did you solve it?
    Do me a favour~~:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I met the same problem...did you solve it?
    Do me a favour~~:)