Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development usage of LWIP with Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 211 views
  • Users 0 members are here
Related

usage of LWIP with Zedboard

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I have a AMP solution working on my Zedboard. One of my cores is running a custom Bare Metal Application and another is running Linux. Now i was want to set up a Inter core communication based on TCP/IP. The Core1 running linux will listen to a socket connection from the Core0 which is running the baremetal application.

Can i use the LWIP stack to open the socket in Core0 which is running a bare metal application for zedboard. So How does this work? Do i just build a statically linked bare metal application with all the LWIP SDK provided or do i need lwip libraries implemented on core0 ( running bare metal).

I also would like to know if this would be a implementable option for Zeboard?