Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux can not get start on the zed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 907 views
  • Users 0 members are here
Related

Linux can not get start on the zed board

e14 Contributor
e14 Contributor over 13 years ago

Hello every one ,
        
      The linux system cannot get start on my board.
      
      There are logs printed through the serial port
U-Boot 2012.04.01-00304-g7639205 (May 11 2013 - 15:43:39)

DRAM:  512 MiB
WARNING: Caches not enabled
MMC:   SDHCI: 0
Using default environment

In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 12
OEM: 3456
Name: F0F0F
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading zImage

2483504 bytes read
reading devicetree.dtb

5793 bytes read
reading ramdisk8M.image.gz

3622263 bytes read
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
           the system stopped here , booting the kernel failed.

           What's the reason causing this kind of problem..

          Hoping your help!

SXL

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hey  sxl630828191,
    Have you followed speedway labs (lab1_1 ,lab1_2 and lab 1_3) for implementing linux on zynq? If you haven't go through them.They have explained how to create boot.bin using zynq_fsbl_0.elf,system.bit and u-boot.elf.It must work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hey  sxl630828191,
    Have you followed speedway labs (lab1_1 ,lab1_2 and lab 1_3) for implementing linux on zynq? If you haven't go through them.They have explained how to create boot.bin using zynq_fsbl_0.elf,system.bit and u-boot.elf.It must work