Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Jumbo Frame Support
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 818 views
  • Users 0 members are here
Related

Jumbo Frame Support

e14 Contributor
e14 Contributor over 13 years ago

I've recently received a ZedBoard and attempted to turn on jumbo frames through both ifconfig(ifconfig eth0 mtu 9000) and the ioctl(ioctl(fd, SIOCSIFMTU, &mtustruct)).  Both gave me a response of an invalid argument.

Are jumbo frames supported on the ZedBoard, or do I need to recompile the kernel?

Thanks

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 13 years ago

    Hi andyg,

    Here a snippet from the header of the r14.5 Xilinx Linux kernel driver source drivers/net/ethernet/xilinx/xilinx_emacps.c:

    /*
    
    * Xilinx Ethernet: Linux driver for Ethernet.
    
    *
    
    * Author: Xilinx, Inc.
    
    *
    
    * 2010 (c) Xilinx, Inc. This file is licensed uner the terms of the GNU
    
    * General Public License version 2. This program is licensed "as is"
    
    * without any warranty of any kind, whether express or implied.
    
    *
    
    * This is a driver for xilinx processor sub-system (ps) ethernet device.
    
    * This driver is mainly used in Linux 2.6.30 and above and it does _not_
    
    * support Linux 2.4 kernel due to certain new features (e.g. NAPI) is
    
    * introduced in this driver.
    
    *
    
    * TODO:
    
    * 1. JUMBO frame is not enabled per EPs spec. Please update it if this
    
    *    support is added in and set MAX_MTU to 9000.

     

    In V1.5 of UG585, Section 16.1.4, there is even further clarification on the Zynq hardware support for Jumbo frames:

     

    Section 16.1.4 Notices

    ...

    Jumbo Frames

    Jumbo frames are not supported

     

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Is there another driver that can be installed in Linux to get Jumbo frames for a Avnet MMP (7z045)?

    Steve Dean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    What exactly is the limitation preventing Jumbo Frames? Is it the Ethernet controller hardware? Can the MTU be set any higher than 1500?

    Steve