Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Problem apllication under linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 388 views
  • Users 0 members are here
Related

Problem apllication under linux

100saber
100saber over 12 years ago

Hello,

i am trying to create a sample code under linux (in the SD card) and when i creat my apllication in SSDK IE i have this :

Building file: ../src/helloworld.c
Invoking: ARM Linux gcc compiler
arm-xilinx-linux-gnueabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"src/helloworld.d" -MT"src/helloworld.d" -o "src/helloworld.o" "../src/helloworld.c"
C:QNX630hostwin32x86usrbinsh.exe: *** heap allocated but not at 0x590000
      0 [main] sh 7928 sync_with_child: child 8996(0x17C) died before initialization with status code 0x1
   3704 [main] sh 7928 sync_with_child: *** child state waiting for longjmp
/cygdrive/c/QNX630/host/win32/x86/usr/bin/sh: arm-xilinx-linux-gnueabi-gcc: Bad address
make: *** [src/helloworld.o] Erreur 1


Can any one help me ?

thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    <p>If you would like to develop your Linux application using the SDK there is an example in the Zynq Concepts, Tools and Techniques tutorial as referenced here: http://www.wiki.xilinx.com/Create+Linux+Application</p>
    <p> </p>
    <p>You can find the Zynq Concepts, Tools and Techniques tutorial to match the version of the Xilinx tools you are using here:</p>
    <p> </p>
    <p>http://www.zedboard.org/design/1521/11</p>
    <p> </p>
    <p>-Gary</p>

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100saber
    0 100saber over 12 years ago in reply to e14 Contributor

    Hello,

    Thanks for your answer. This example shows how pre-built a linux image using u-boot which means booting Linux on one CPU. Whant i am trying to do is running zImage Linux on the Zynq dual core. The examples provided descrive only u-boot.
    I didn't find examples that show how to generate a new OS image ?
    Or how to configure the current image for dual core -SMP.