Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development EGPIO access is too slow to be useful
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 503 views
  • Users 0 members are here
Related

EGPIO access is too slow to be useful

e14 Contributor
e14 Contributor over 13 years ago


I'm doing some timing tests using MicroZed board.
I need to know the maximum data rate from PS to GPIO or EGPIO.

I have a logic analyzer connected to PIO.J5.
I written a C program that writes directly to MIO.DATA_0 regiseters (see code below)

I measure 60ns-120ns per access (write to GPIO0->DATA_0)

This is less than 10 Mhz!!
 
How can I acheive sustained 100Mhz data rate to PL if
the fastest I can push data from PS is < 10Mhz?

What am I doing wrong???

How do I speed up the STR command ???


//------------ C code source ------------------------

fd = open("/dev/mem", O_RDWR | O_SYNC)) == -1) FATAL;

// mmap the MicroZed GPIO page

target = GPIO_BASEADDR ;  // physical ARM IO registers
map_base = mmap(
   0,                      // caddr_t addr
   GPIO_SIZE,              // size_t len = 4K =4096 = 0x1000 Bytes
   PROT_READ | PROT_WRITE, // int prot
   MAP_SHARED,             // int flags
   fd,                     // int filehandle
   target & ~GPIO_MASK     // off_t offset
   );


microzed_gpio = (microzed_gpio_t *)(map_base) ;
volatile unsigned long *gpio_dout0 = &(microzed_gpio->dout0) ;
volatile unsigned long *gpio_dout1 = &(microzed_gpio->dout1) ;

...
...

while( microzed_gpio->DIN1.b19 != 1 ) {

    *(gpio_dout0) = D0_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D1_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D2_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D3_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D4_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D5_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D6_MASK ;
    *(gpio_dout0) = 0  ;

    *(gpio_dout0) = D7_MASK ;
    *(gpio_dout0) = 0  ;

    }

//-------while loop dissambled code -------------
198                .L19:
199 01ac 40B084E5    str     fp, [r4, #64] // 60nS
200 01b0 403084E5    str     r3, [r4, #64] // 60ns
201 01b4 40A084E5    str     r10, [r4, #64]
202 01b8 403084E5    str     r3, [r4, #64]
203 01bc 409084E5    str     r9, [r4, #64]
204 01c0 403084E5    str     r3, [r4, #64]
205 01c4 408084E5    str     r8, [r4, #64]
206 01c8 403084E5    str     r3, [r4, #64]
207 01cc 407084E5    str     r7, [r4, #64]
208 01d0 403084E5    str     r3, [r4, #64]
209 01d4 400084E5    str     r0, [r4, #64]
210 01d8 403084E5    str     r3, [r4, #64]
211 01dc 40E084E5    str     lr, [r4, #64]
212 01e0 403084E5    str     r3, [r4, #64]
213 01e4 40C084E5    str     ip, [r4, #64]
214 01e8 403084E5    str     r3, [r4, #64]
215 01ec 641092E5    ldr     r1, [r2, #100]
216 01f0 020711E3    tst     r1, #524288
217 01f4 ECFFFF0A    beq     .L19

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    You should be using one of the AXI connections to PL. GPIO is going to be slow.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to bhfletcher

    This is a test of the slowest way.
    I'm using it to compare it to other (non-fpga) ARMs
    I'll report the speed improvent when I the the
    AXI PL fifo working.

    I still would like to know if I can get the Slowest, (Software Only) running faster.

    Maybe I've got the clocks setup wrong? Or maybe I've got some bridge priority set wrong?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I've generated a new BitStream with the AXI GPIO in PL.
    Now I need to have the MicroZed boot this instead of the original (system.bit). 
    How do I do this?
    I'm having trouble finding the necessary HOWTOs for BitStreams and Liunx. Any help would be great.