Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to read ramdisk
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 365 subscribers
  • Views 1795 views
  • Users 0 members are here
Related

Unable to read ramdisk

e14 Contributor
e14 Contributor over 13 years ago

With the Speedway tutorial lab2_3, I am facing issues with ramdisk creation. I am booting from the SD card and get the following error message:
zynq-uboot>

U-Boot 2012.10 (Mar 02 2013 - 13:11:18)

DRAM:  512 MiB
WARNING: Caches not enabled
MMC:   SDHCI: 0
SF: Detected S25FL256S with page size 64 KiB, total 32 MiB
SF: Warning - Only lower 16MB is accessible in 3 byte addressing mode
In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 12
OEM: 3456
Name: SMI
Tran Speed: 50000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading uImage

2883984 bytes read
reading devicetree.dtb

7284 bytes read
reading ramdisk32M.image.gz

** Unable to read "ramdisk32M.image.gz" from mmc 0:1 **
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux-3.6.0-xilinx
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2883920 Bytes = 2.8 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
Wrong Ramdisk Image Format
Ramdisk image is corrupt or invalid

------------------------------------------
If I print the environment variables this is what I see:
zynq-uboot>
zynq-uboot> printenv
baudrate=115200
bootcmd=run modeboot
bootdelay=3
devicetree_image=devicetree.dtb
devicetree_size=0x20000
ethact=zynq_gem
ethaddr=00:0a:35:00:01:22
fdt_high=0x20000000
filesize=88C08C
initrd_high=0x20000000
ipaddr=192.168.0.99
jtagboot=echo TFTPing Linux to RAM...;tftp 0x3000000 ${kernel_image};tftp 0x2A00000 ${devicetree_image};tftp 0x2000000 ${ramdisk_image};bootm 0x3000000 0x2000000 0x2A00000
kernel_image=uImage
kernel_size=0x500000
modeboot=run sdboot
nandboot=echo Copying Linux from NAND flash to RAM...;nand read 0x3000000 0x100000 ${kernel_size};nand read 0x2A00000 0x600000 ${devicetree_size};echo Copying ramdisk...;nand read 0x2000000 0x620000 ${ramdisk_size};bootm 0x3000000 0x2000000 0x2A00000
norboot=echo Copying Linux from NOR flash to RAM...;cp 0xE2100000 0x3000000 ${kernel_size};cp 0xE2600000 0x2A00000 ${devicetree_size};echo Copying ramdisk...;cp 0xE2620000 0x2000000 ${ramdisk_size};bootm 0x3000000 0x2000000 0x2A00000
qspiboot=echo Copying Linux from QSPI flash to RAM...;sf probe 0 0 0;sf read 0x3000000 0x100000 ${kernel_size};sf read 0x2A00000 0x600000 ${devicetree_size};echo Copying ramdisk...;sf read 0x2000000 0x620000 ${ramdisk_size};bootm 0x3000000 0x2000000 0x2A00000
ramdisk_image=ramdisk32M.image.gz
ramdisk_size=0x2000000
sdboot=echo Copying Linux from SD to RAM...;mmcinfo;fatload mmc 0 0x3000000 ${kernel_image};fatload mmc 0 0x2A00000 ${devicetree_image};fatload mmc 0 0x2000000 ${ramdisk_image};bootm 0x3000000 0x2000000 0x2A00000
serverip=192.168.0.101
stderr=serial
stdin=serial
stdout=serial

Environment size: 1589/131068 bytes

I am a newbie to linux and will appreciate some help with this.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • 100padudle
    0 100padudle over 12 years ago

    Hello All,

    I am trying to boot linux on a MicroZed board.  When I boot from the SD Card I get the following errors.

    zynq-uboot> boot
    Device: zynq_sdhci
    Manufacturer ID: 2
    OEM: 544d
    Name: SA04G
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 3.7 GiB
    Bus Width: 4-bit
    reading uEnv.txt
    ** Unable to read file uEnv.txt **
    Copying Linux from SD to RAM...
    reading uImage
    ** Unable to read file uImage **
    zynq-uboot>

    I am compiling from the source on the Xilinx github

    Here is my bootgen .bif file:

    image : {
            [bootloader]fsbl_uzed.elf
            u-boot.elf
            [load=0x2a00000]zynq-zed.dtb
            [load=0x2000000]uramdisk.image.gz
            [load=0x3000000]uImage.bin   // currently bootgen requires a file extension. this is just a renamed uImage
    }

    I do have the mkimage utility available so I believe the linux make command creates the u-boot wrapped kernel image uImage.  I rename it to uImage.bin to make bootgen happy.

    When I run the file command on uImage.bin I get this output:

    uImage.bin: u-boot legacy uImage, Linux-3.14.0-xilinx, Linux/ARM, OS Kernel Image (Not compressed), 3334192 bytes, Wed Jun 18 10:14:31 2014, Load Address: 0x00008000, Entry Point: 0x00008000, Header CRC: 0x24A5CF28, Data CRC: 0x8E1040F6


    Can anyone tell me what I am doing wrong or what to try?

    Thanks,

        Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100padudle
    0 100padudle over 12 years ago

    Hello All,

    I am trying to boot linux on a MicroZed board.  When I boot from the SD Card I get the following errors.

    zynq-uboot> boot
    Device: zynq_sdhci
    Manufacturer ID: 2
    OEM: 544d
    Name: SA04G
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 3.7 GiB
    Bus Width: 4-bit
    reading uEnv.txt
    ** Unable to read file uEnv.txt **
    Copying Linux from SD to RAM...
    reading uImage
    ** Unable to read file uImage **
    zynq-uboot>

    I am compiling from the source on the Xilinx github

    Here is my bootgen .bif file:

    image : {
            [bootloader]fsbl_uzed.elf
            u-boot.elf
            [load=0x2a00000]zynq-zed.dtb
            [load=0x2000000]uramdisk.image.gz
            [load=0x3000000]uImage.bin   // currently bootgen requires a file extension. this is just a renamed uImage
    }

    I do have the mkimage utility available so I believe the linux make command creates the u-boot wrapped kernel image uImage.  I rename it to uImage.bin to make bootgen happy.

    When I run the file command on uImage.bin I get this output:

    uImage.bin: u-boot legacy uImage, Linux-3.14.0-xilinx, Linux/ARM, OS Kernel Image (Not compressed), 3334192 bytes, Wed Jun 18 10:14:31 2014, Load Address: 0x00008000, Entry Point: 0x00008000, Header CRC: 0x24A5CF28, Data CRC: 0x8E1040F6


    Can anyone tell me what I am doing wrong or what to try?

    Thanks,

        Pete