Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development peripheral tests LEDs blinking problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 195 views
  • Users 0 members are here
Related

peripheral tests LEDs blinking problem

e14 Contributor
e14 Contributor over 13 years ago

I have successfully created a hello world project. The problem comes when I create a Peripheral test project. It works fine, but I believe that the LEDs should be blinking, which they don't. The system only returns that all the peripherals are working correctly. I have even modified the source code to print out which LED should be illuminated. I am using ISE 14.6 and at the planahead project I checked and the UCF for the LEDs is correct.

#
# pin constraints
#
NET GPIO_SW_TRI_IO LOC = "G19"  |  IOSTANDARD = "LVCMOS25";
NET LEDs_4Bits_TRI_IO[0] LOC = "P17"  |  IOSTANDARD = "LVCMOS25";
NET LEDs_4Bits_TRI_IO[1] LOC = "P18"  |  IOSTANDARD = "LVCMOS25";
NET LEDs_4Bits_TRI_IO[2] LOC = "W10"  |  IOSTANDARD = "LVCMOS25";
NET LEDs_4Bits_TRI_IO[3] LOC = "V7"  |  IOSTANDARD = "LVCMOS25";
#
# additional

Any idea what might be wrong?