Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UART-0 interrupt and freertos
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 904 views
  • Users 0 members are here
Related

UART-0 interrupt and freertos

fayyazrafiq
fayyazrafiq over 13 years ago

Dear All,

Has anybody configure interrupts  for zynq in freertos environment. I tried UART-0 interrupt but my interrupt never hits. Could anybody share some sample code for any interrupt in freertos environment.
Any help is highly appreciated.

Regards
M. Fayyaz

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I was able to implement the FPGA interrupt ( 91) which is a SPI and i suppose you could do the same for UART as well.

    I did the following

    The interrupt controller is already initialized for the TICK interrupt. So i used

    prvGetInterruptControllerInstance();

    to get a instance of the same in my main function. Then I connected my SPI interrupt with the controller using

    XScuGic_Connect

    I enabled the interrupt using

    XScuGic_Enable(InterruptController, 91);

    After that I set the Target CPU ( in my case CPU1) using

    CpuID = XSCUGIC_SPI_CPU1_MASK;
    CpuID |= CpuID << 8;
    CpuID |= CpuID << 16;

    XScuGic_DistWriteReg(InterruptController,XSCUGIC_SPI_TARGET_OFFSET_CALC(91),CpuID);

    Then it works. I hope you can do the same for UART since it is also a SPI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I was able to implement the FPGA interrupt ( 91) which is a SPI and i suppose you could do the same for UART as well.

    I did the following

    The interrupt controller is already initialized for the TICK interrupt. So i used

    prvGetInterruptControllerInstance();

    to get a instance of the same in my main function. Then I connected my SPI interrupt with the controller using

    XScuGic_Connect

    I enabled the interrupt using

    XScuGic_Enable(InterruptController, 91);

    After that I set the Target CPU ( in my case CPU1) using

    CpuID = XSCUGIC_SPI_CPU1_MASK;
    CpuID |= CpuID << 8;
    CpuID |= CpuID << 16;

    XScuGic_DistWriteReg(InterruptController,XSCUGIC_SPI_TARGET_OFFSET_CALC(91),CpuID);

    Then it works. I hope you can do the same for UART since it is also a SPI