Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Android
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1135 views
  • Users 0 members are here
Related

Android

e14 Contributor
e14 Contributor over 14 years ago

Is there a way to implement the following design?

1) Run C code generated from Matlab in a real-time bare metal configuration on Arm core 0.

2) Run Android on Arm core 1 which will peek and poke data from the programmable logic and Arm core 0 and send it out to the PC via ethernet, or display it via a touchscreen.

3) Run custom or Matlab HDL Coder generated VHDL on the programmable logic.

The programmable logic and Arm core 0 are running real time application code and Android serves as a non real time interface between the host PC or visualization equipment.

I would like to get started on a design that implements this technology and am wondering if there is anybody out there willing to struggle through this with me.  Thanks for your time.

  ,Doctor K



  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    1. The Matlab real-time compiler can be pretty finicky when it comes to writing usable C/C++ code.  If you follow their recommended programming guide for embedded code, then yes it will run without a problem.

    2. I would recommend booting into Android on Core 0 and running the real-time code on Core 1.  This will make booting much much simpler.  Either way, both configurations are valid.

    3. Matlab HDL Coder produces HDL (VHDL or Verilog) code that is human readable.  You would then synthesize the code with ISE or PlanAhead and put it into the Programmable Logic portion of Zynq.

    Is there a specific reason why you want to use Android rather than a real-time port of Linux?

    -TD

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    1. The Matlab real-time compiler can be pretty finicky when it comes to writing usable C/C++ code.  If you follow their recommended programming guide for embedded code, then yes it will run without a problem.

    2. I would recommend booting into Android on Core 0 and running the real-time code on Core 1.  This will make booting much much simpler.  Either way, both configurations are valid.

    3. Matlab HDL Coder produces HDL (VHDL or Verilog) code that is human readable.  You would then synthesize the code with ISE or PlanAhead and put it into the Programmable Logic portion of Zynq.

    Is there a specific reason why you want to use Android rather than a real-time port of Linux?

    -TD