Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xillinux-1.3 is out!
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 332 views
  • Users 0 members are here
Related

Xillinux-1.3 is out!

e14 Contributor
e14 Contributor over 12 years ago

Hi,

An updated version of Xillinux is now available for download. It's pretty similar to the existing Linux distribution, but has a few advantages:

* Supports Zedboard, MicroZed and ZyBo.
* Easier FPGA (PL) development cycle: The programming file in *.bit format is copied to the SD card, rather than generating the boot.bin file.
* The Xillybus IP core relies on the ACP port, allowing for higher data bandwidth (~ 300 MB/s) and a significantly lower I/O related CPU consumption.
* Rebooting is supported (as opposed to only shutdown / halt).
* Linux kernel updated from version 3.3.0 to 3.12.0
* U-boot upgrade, with more options
* Capability of setting the board's Ethernet MAC address permanently, instead of the default

For more information about upgrading,

http://xillybus.com/doc/old-xillinux-zedboard

To download the new version:

http://xillybus.com/xillinux

Cheers,
   Eli

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Is it possible install the Python and Octave in Xillinux?

    I try do as a Ubuntu 12.04, but it isn't work. Do we need do anything more?