Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linaro
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 363 subscribers
  • Views 1433 views
  • Users 0 members are here
Related

Linaro

e14 Contributor
e14 Contributor over 14 years ago

I have been introduced to Linaro recently http://www.linaro.org/ .  I enjoy the consistency of a toolchain and community there.  While I am aware there will be the same for the Zedboard, does anyone have any ideas of incorporating the Linaro tools over as well?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I'm also trying to make it work, at the moment the things i've done are:
    - add a second partition (ext2) to the CF
    - uncompress the linaro fs image in the CF
    - start the original linux from the CF
    - mount the linaro fs to /mnt:
      mount /dev/mmcblk0p2 /mnt
    - mount the /proc:
      mount none /mnt/proc -t proc
    - chroot to the linaro fs:
      chroot /mnt
    at this point most of the linaro applications works
    if you execute them, for example:
      ifconfig eth0 down
      dhclient eth0 &
      ifconfig eth0 up

    but i'm sure this is NOT the way to do it!
    there must be a way to call the (linaro) init process
    after chroot but i can't still see how.

    Can enyone enlighten us?

    Bye, C.


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    claudio.lorini,

    Take a look at this post:

    http://zynqgeek.blogspot.com/2012/09/modify-your-boot-image-on-your-zedboard.html

    It goes through modifying your SD-Card image.  I believe that is what you would like to do here, modify the RAM Disk image to mount the second partition, rather than mount the /proc and other partitions in RAM.

    Hope that helps!  Let me know if you get it working, and if not I'll do a write-up on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you ZG,
    i was trying to avoid using the ramdisk and use a regular FS in CF in order to make the modification to the system permanent.
    I suceeded when i realized thet the u-boot wasn't correctly passing the kernel parameters... anyway the ext4 fs on cf doesn't seem to be very robust, during usage you get a lot of IO errors and the FS gets corrupted, so the ramdisk isn't a bad idea after all!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I am getting tons of IO errors on my Zed SD card as well, but they appeared before and ext fs touched the card. 

    Is there some reason to expect that ext4 on SD is not robust or is the SD card just bad (both of ours??)?

    I'd also like to get away from the ramdisk scenario, but have run into this.  I am a bit of a linux noob, so it's not entirely clear how to get there from here, but these IO errors just seem wrong. :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    In my opinion the IO errors are probably hw related, i've tried different brands of CF and there are differences in the quantity of errors you get. With the best one i managed to run a couple of hours without errors, but you have to wait long enough and there you are.
    Next thing i'd like to try is to mount the FS on a USB stick and see what happens... I'll let you know...
    C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    In my opinion the IO errors are probably hw related, i've tried different brands of CF and there are differences in the quantity of errors you get. With the best one i managed to run a couple of hours without errors, but you have to wait long enough and there you are.
    Next thing i'd like to try is to mount the FS on a USB stick and see what happens... I'll let you know...
    C.