Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problem of PS UART self-test application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 365 subscribers
  • Views 1616 views
  • Users 0 members are here
Related

problem of PS UART self-test application

e14 Contributor
e14 Contributor over 13 years ago

Hi...
I have faced a strange problem.
I use the code that Xilinx offers, named xuartps_selftest_example.c, and don't modify it except some instance name. When I run it, it shows unrecognizable code and shows Failed. But when I debug it, it shows success.
What's the problem?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 13 years ago

    Hi tec998s,

    Which version of tools are you using?  Can you describe the failure any further?  When you say that the application "shows unrecognizable code and shows Failed" are you referring to garbled output on the console?

    When you run the application, are you creating a new run configuration for the application?

    If the UART1 PS device is not being initialized properly to generate character outputs at the correct baud rate, this condition could cause garbled characters on the console.

    The ps7_init.tcl file exported into SDK by PlanAhead is used by XMD in the background to initialize the Zynq PS hardware before executing an application.  I know that by default, when creating a debug configuration, the path to the ps7_init.tcl gets populated in the "Device Initialization" tab of the
    Debug Configurations manager.  Can you check to see if that same ps7_init.tcl file is being specified for your application's Run Configuration as well?

    Also, I would recommend against using the serial console built into SDK for now.  I recommend using the latest version of Tera Term which is available for free from the SourceForge Japan site:

    http://ttssh2.sourceforge.jp/index.html.en

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    I have a similar UART problem.  I routed the PS uart0 to the EMIO and then to two PMOD pins, JA1 and JA2,   The stdin and stdout for the BSP are set to ps7_uart_1 and the through the Cypress usb to serial chip as per the standard config.  The default baud rate  for stdout /stdin is specified as 115200. But after adding UART0, It seems to step down to half the baud rate of 57600. (using Terra term)    Then the loopback test for the UART0 fails for both the polled mode and interrupt mode. Running the debugger shows the return test string misaligned as if the loopback mode is broken.
    I'm using  Plan Ahead/EDK/SDK 14.3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    I have a similar UART problem.  I routed the PS uart0 to the EMIO and then to two PMOD pins, JA1 and JA2,   The stdin and stdout for the BSP are set to ps7_uart_1 and the through the Cypress usb to serial chip as per the standard config.  The default baud rate  for stdout /stdin is specified as 115200. But after adding UART0, It seems to step down to half the baud rate of 57600. (using Terra term)    Then the loopback test for the UART0 fails for both the polled mode and interrupt mode. Running the debugger shows the return test string misaligned as if the loopback mode is broken.
    I'm using  Plan Ahead/EDK/SDK 14.3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fayyazrafiq
    0 fayyazrafiq over 12 years ago in reply to e14 Contributor

    I am getting the same problem, could you please tell me, how you resolved the problem.

    Many Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to fayyazrafiq

    I have the same problem.  I routed UART0 from the PS to the PL through the EMIO.  The self test is failing.  Did anyone figure out a fix?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fayyazrafiq
    0 fayyazrafiq over 12 years ago in reply to e14 Contributor

    I am facing the same problem, i routed the UART0 to EMIO and then to package pins but no data output. I am using XPS/SDK 14.5. I wrote somewhere that it is bug in the ZEDBOARD (http://www.zedboard.org/content/zedboard-revision-d-bug-issues-emio-related). I found so many posts for this problem but there is no single solution exist either from Xilinx or ZEDBOARD side. I thought either the ZEDBOARD manufacturer or the XILINX are concealing something which is very severe and wasting time for the developer in this field.