Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problem of PS UART self-test application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 365 subscribers
  • Views 1612 views
  • Users 0 members are here
Related

problem of PS UART self-test application

e14 Contributor
e14 Contributor over 13 years ago

Hi...
I have faced a strange problem.
I use the code that Xilinx offers, named xuartps_selftest_example.c, and don't modify it except some instance name. When I run it, it shows unrecognizable code and shows Failed. But when I debug it, it shows success.
What's the problem?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I hope that this is of some help. I am using Vivado 2014.2 with the ZC702 board (not the ZedBoard), but I think that my solution may work for ZedBoard as well. I saw the comment by Kevin above about the ps7_init.tcl file and it led me to check which ps7_init.tcl was used in my debug and in my run configurations. It turns out that Vivado/SDK2014.2 automatically populated the configurations with the wrong file, from an old design. I switched to the ps7_init.tcl file in the <design>/<design>.sdk/<design>_hw_platform_0/ps7_init.tcl and the UART test suddenly started passing.

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I hope that this is of some help. I am using Vivado 2014.2 with the ZC702 board (not the ZedBoard), but I think that my solution may work for ZedBoard as well. I saw the comment by Kevin above about the ps7_init.tcl file and it led me to check which ps7_init.tcl was used in my debug and in my run configurations. It turns out that Vivado/SDK2014.2 automatically populated the configurations with the wrong file, from an old design. I switched to the ps7_init.tcl file in the <design>/<design>.sdk/<design>_hw_platform_0/ps7_init.tcl and the UART test suddenly started passing.

    Paul