Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Power Cycle Problems
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 555 views
  • Users 0 members are here
Related

Power Cycle Problems

e14 Contributor
e14 Contributor over 14 years ago

Every time I shut down the Zedboard while it's running Xillinux, no matter how I shut it down (turn off system, restart system, flip the switch), it fails to reload properly.  It gives the following message repeatedly upon startup:

init: Failed to create pty - disabling logging for job

and then does nothing.  I believe this is an issue because of the non-standard /dev setup, however I haven't seen anyone else post this problem.  There is no command line so I cannot try terminal commands.  ctrl+alt+delete resulted in it telling me it cannot find the device-mapper in /proc/misc, then says it will restart and does nothing.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Apparently I'm only having this issue after installing OpenCV.  OpenCV just doesn't want to cooperate with the ZedBoard, it seems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Okay, I think I figured out *what* the problem is, although I'm unsure how to rectify it.  When I do apt-get upgrade, it changes the initramfs to look for modules in the 3.2.0-omap4 directory instead of the 3.3.0-xillinux-1.0 directory (or maybe it was like this before, but there seems to be some confusion as to which kernel to use sometimes).  I'm fairly certain it has something to do with initramfs, and I'm curious how I can modify this appropriately.  If I force it to update itself, it links itself to the omap4 kernel instead of the xillinux kernel, which is why I believe I'm having so many issues.  Does this make sense to anybody and does anybody know what to do about this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Yeah, so apt-get upgrade links to the old omap4 kernel which is bad.  You can fix this by going to /boot and

    $rm vmlinuz

    which will delete the link to the old kernel.  To make a link to the new one, use

    $ln -s vmlinuz-3.3.0-xillinux-1.0 vmlinuz

    Apparently I'm the only person having this problem, but if that's not true (and I don't see how it could be since it's a brand new board and we should all be starting with the same image) it's pretty annoying that you can't use standard terminal commands with something that's supposed to be a full linux distro without causing boot problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    As I've said in another post, Xillinux wasn't intended to be apt-upgraded. It seems like the attempt to upgrade altered the boot chain, which diverts from Ubuntu's. Or messed something else up.