Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Bare metal USB device code
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 1019 views
  • Users 0 members are here
Related

Bare metal USB device code

e14 Contributor
e14 Contributor over 14 years ago

as subject, anybody done or aware of code that implement any minimal work usb device mode stack on zynq?

sure its ARM and EHCI so some generic code is available, but I wonder if there is any code that has actually been verified to work on zynq-zedboard?

Antti

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I am curious about this as well. There is a sample project available in the xilinx SDK documentation which is supposed to act like a USB mass storage device. I have tried it and I can get it to compile and run, but I can't get my host PC to detect anything when I connect it. Also, no interupts fire on my device either.

    If it will help you, the example code is installed on your machine here for 14.3 "Xilinx_install_dir/14.3/ISE_DS/EDK/sw/XilinxProcessorIPLib/drivers/usbps_v1_03_a/examples/". Similar examples are available in similar locations for 14.2 and 14.1 as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    This code does work. I got some code from a local Avnet technical marketing guy which helped me get it working for my ZC702 board. The USB PHY needed to be reset before it would work. So this code snippet placed at the beginning of main() did the trick:

        // The following code is required for ZC702 (Rev C tested) to place USB PHY out of reset.
        // this block of code needed is not needed for the ZedBoard (Rev B tested)
        Xil_Out32(0xe000a204, 0x80);
        Xil_Out32(0xe000a208, 0x80);
        Xil_Out32(0xe000a040, 0x80);
        Xil_Out32(0xe000a040, 0x00);
        Xil_Out32(0xe000a040, 0x80);

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    This code does work. I got some code from a local Avnet technical marketing guy which helped me get it working for my ZC702 board. The USB PHY needed to be reset before it would work. So this code snippet placed at the beginning of main() did the trick:

        // The following code is required for ZC702 (Rev C tested) to place USB PHY out of reset.
        // this block of code needed is not needed for the ZedBoard (Rev B tested)
        Xil_Out32(0xe000a204, 0x80);
        Xil_Out32(0xe000a208, 0x80);
        Xil_Out32(0xe000a040, 0x80);
        Xil_Out32(0xe000a040, 0x00);
        Xil_Out32(0xe000a040, 0x80);

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    You find the key, and now my project works well. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100alfi
    0 100alfi over 9 years ago in reply to e14 Contributor

    Hello Dangmug .

    i am trying to establish a connection between zynq7000 and usb2.0 Phy IC , I Need a source code for windows side for host device .i tried to google but i did not find a right code .your feedback will be greatly appreciated .

    Thank you