Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development u-boot compilation errors
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 364 subscribers
  • Views 1466 views
  • Users 0 members are here
Related

u-boot compilation errors

satishkumar
satishkumar over 11 years ago

Dear all,

I am downloading u-boot code from following link,
https://github.com/Xilinx/u-boot-xlnx

with "git clone https://github.com/Xilinx/u-boot-xlnx.git"
I am trying to compile with

make ARCH=arm zynq_zed_config
make ARCH=arm

I am getting error as

"In file included from tools/aisimage.c:10:0:
include/image.h:880:27: fatal error: openssl/evp.h: No such file or directory"

can you please help me out to resolve the problem.

Thanks & Regards
Satish.G


  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Satish,

      Did you check out a specific tag?  Are you using the Code Sourcery or Linaro toolchain?  To make sure you didn't miss any steps, take a look at the Ubuntu Tutorial for ZedBoard chapter on Creating the Second Stage loader.   The information there is still relevent.  

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • satishkumar
    0 satishkumar over 11 years ago

    I am using arm-xilinx-linux-gnueabi- for compiling u-boot which default provided with Vivado.
    I will try with code sourcery

    --Satish.G

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    That is the Code sourcery toolchain.  I've used both many times without a problem, but I haven't built anything lately specifically for Zedboard.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I just ran into this exact issue and found a solution. It turns out I was missing the openssl library. To get it, I did:
    yum install openssl-devel.x86_64
    (P.S. This should work on CentOS/RedHat. You'll need to find the equivalent for your system if it's something else.)
    (P.P.S. You should do this as root/sudo to avoid permission issues.)

    I had originally just installed the 32-bit library by doing:
    yum install openssl-devel.i686
    That cleared the header issue, but gave the following error when it tried to link:
    /usr/bin/ld: skipping incompatible /usr/lib/gcc/x86_64-redhat-linux/4.4.7/../../../libssl.so when searching for -lssl
    /usr/bin/ld: skipping incompatible /usr/lib/libssl.so when searching for -lssl

    The smoking gun that told me I needed the 64-bit lib was where it says "x86_64".

    Under no circumstance should you try downloading the openssl sources and compiling/cross-compiling them yourself. It was a complete waste of time.

    BTW - I am using Code Sourcery/Petalinux tool chain -- although this error is coming from the HOST tool chain.

    Hope this helps...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I am getting exactly the same error as described by Satish while compiling PetaLinux U-boot. As we are getting that error from the arm-xilinx-linux-gnueabi- tool chain, no host tool chain, lib or include file is involved. This is still an open problem.

    -Gordon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    My bad. You are correct in everything you said. I apologize profusely )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    thx! This was the solution for the prob. I downloaded openssl devel rpm for my opensuse distro and the compilation did run through without any errors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    FWIW, the corresponding Debian/Ubuntu package is "libssl-dev".