Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Where does the Kernel command line come from?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 345 views
  • Users 0 members are here
Related

Where does the Kernel command line come from?

e14 Contributor
e14 Contributor over 12 years ago

I would like to modify the behaviour of the XiLinux 3.8.0 kernel on the MicroZed board slightly.

While The board boots from the SD card I see the following command line:

Kernel command line: console=ttyPS0,115200 root=/dev/ram rw ip=192.168.1.10 earlyprintk

I assume the line is generated by U-BOOT when it activates/starts the kernel.

The actual parameters being passed come from "bootargs". The only plave where I can find anything like that is in the file "devicetree-microzed-sdio 125mhz-4gbram-PHY-LED.dts" on the SD card.
I have tried modifying it there (adding mem=800M to the bootargs in it) but that does not make a difference.

So: how do I get it done? rebuild U-BOOT? If so where do you define what gets passed ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    Yes, the kernel command line is indeed in the dts file on Xillinux. Note that the dtc compiler is installed in the kernel's headers on Xillinux' file system (look in /usr/src/kernels/, so if you're able to boot Xillinux, you may compile the new dts on the board itself.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello,

    Yes, the kernel command line is indeed in the dts file on Xillinux. Note that the dtc compiler is installed in the kernel's headers on Xillinux' file system (look in /usr/src/kernels/, so if you're able to boot Xillinux, you may compile the new dts on the board itself.

    Regards,
       Eli