Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development avnet mini itx board u-boot problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 651 views
  • Users 0 members are here
Related

avnet mini itx board u-boot problem

e14 Contributor
e14 Contributor over 12 years ago

Hi
I have an u-boot problem on avnet zynq mini itx board:

I rebuild the latest u-boot image fromuFF1Agit clone git://git.xilinx.com/u-boot-xlnx.git, and found that sometimes it boot fail on my Avnet mini itx board(Mini-itx-7z-asy-g), it may hang in boot early stage like below:

U-Boot 2014.01-dirty (Jun 24 2014 - 15:29:02)

I2C: ready
Memory: ECC disabled
DRAM: 1 GiB
MMC: zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB

Of course, the pre-flash u-boot(U-Boot 2013.01-dirty) in the SD card from the vendor does not have the problem, and I have a "2013.04" version, it does not have the problem either.

It should be a software issue and it seems that the later u-boot version have the problem. And I also test the 2014.01-dirty version on ZC706 board, it does not have the problem.

Would you please help me with this problem? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Gary

    Thanks for your help, I do not only need the working u-boot image but also the latest u-boot source code, as I want to change the u-boot code to re-make a u-boot image. Would you please tell me how can I get the u-boot source code for mini itx and the steps to rebuild it? Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Gary

    Thanks for your help, I do not only need the working u-boot image but also the latest u-boot source code, as I want to change the u-boot code to re-make a u-boot image. Would you please tell me how can I get the u-boot source code for mini itx and the steps to rebuild it? Thanks!