Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development configuring axi_gpio interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 532 views
  • Users 0 members are here
Related

configuring axi_gpio interrupt

e14 Contributor
e14 Contributor over 13 years ago

Hi everyone,

using the example codes in SDK, I've managed to handle swtiches & leds connected to axi_gpio in an interrupt routine.

I'd like now to configure the interrupt in such way:
1)only 1 or 2 bit trigger the interrupt (now every bit in the gpio channel trigger it);

2)only the edge low to high triggers the interrupt (now every change status triggers the interrupt)

how can I do these configurations? where can I find information?

thanks in advance!

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    In looking at DS744, it doesn't appear that the current AXI_GPIO can do what you want. You can independently enable each of the two possible channels, but not the individual bits inside those channels. I also don't see that there is any control over the trigger mechanism.

     

    I suggest you open a support case with Xilinx to see if they have a modified version of this core internally that accomplishes this.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    thanks a lot for the answer.
    I will use the axi_intc controller, it allows all the configurations I need

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I post here my question so I don'T have to open a new thread.
    I'm trying to configure the axi_intc controller but in XPS the fields "C_KIND_OF_INTR", "C_KIND_OF_EDGE" AND "C_KIND_OF_LEVEL" are fixed at 0xffffffff and they aren't editable.
    why happens that?