Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Can't boot linaro kernel
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 980 views
  • Users 0 members are here
Related

Can't boot linaro kernel

joswa
joswa over 13 years ago

I've tried to follow the tutorial, "Ubuntu_on_Zedboard_Tutroial_v14.4_01.pdf" to build ubuntu on zedboard with adv7511. However, after running the u-boot and load the kernel, the following error got and the kernel hangs,



** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.

Error: unrecognized/unsupported machine ID (r1 = 0x0fb71dd0).

Available machine support:

ID (hex)        NAME
00000d32        Xilinx Zynq Platform

Please check your kernel config and/or bootloader



I've exactly followed the tutorial. All the u-boot.bin, zImage and devicetree.dtb are successfully built.



Any suggestion what's wrong?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    I'm tryng to use Linaro with kernel linux-3.6-digilent
    and I cannot boot correctly from SDRAM
    -
    when I compile the kernel with option:
    make ARCH=arm xilinx_zynq_defconfig
    -
    and CONFIG_XILINX_FIXED_DEVTREE_ADDR=y
    then booting the uImage with the on-ram fs hangs after writing:
    Calibrating delay loop...
    -
    but if I boot the zImage and the linaro fs on 2nd partition it boots and when the boot ends
    it starts an endless printout of:
    watchdog watchdog0: watchdog did not stop!

    if CONFIG_XILINX_FIXED_DEVTREE_ADDR is not set
    then booting the uImage with the on-ram fs is OK
    -
    but if I boot the zImage and the linaro fs on 2nd partition
    it generates the unrecognized/unsupported machine ID (r1=0x1fb6c62c)
    and says that the ID should be 00000d32
    -
    (I did configure the #define CONFIG_MACH_TYPE 0xd32 in u-boot,
    but this doesn't work)
    -
    when I compile the kernel with option:
    make ARCH=arm digilent_zed_defconfig
    -
    if CONFIG_XILINX_FIXED_DEVTREE_ADDR=y
    then booting the uImage with the on-ram fs hangs after writing:
    Uncompressing Linux... done, booting the kernel.
    -
    booting the zImage and the linaro fs on 2nd partition
    it starts an endless printout of:
    [  ss.cc0000]watchdog watchdog0: watchdog did not stop!
    if CONFIG_XILINX_FIXED_DEVTREE_ADDR is not set
    then booting the uImage with the on-ram fs is OK
    -
    if I boot the zImage and the linaro fs on 2nd partition it hangs after writing:
    Uncompressing Linux... done, booting the kernel.
    -
    in conclusion Linaro (or a FS from the 2nd partition) is usable only with the zImage from linux-3.3
    -
    how to fix the watchdog problem?
    it is very complicated to use the FS on ram and loosing everything at each turn-off
    I even tried to use linux-digilent-dev-3.8, with the same results;
    anyway within that Makefile there is the old 3.6.0 indication

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    I'm tryng to use Linaro with kernel linux-3.6-digilent
    and I cannot boot correctly from SDRAM
    -
    when I compile the kernel with option:
    make ARCH=arm xilinx_zynq_defconfig
    -
    and CONFIG_XILINX_FIXED_DEVTREE_ADDR=y
    then booting the uImage with the on-ram fs hangs after writing:
    Calibrating delay loop...
    -
    but if I boot the zImage and the linaro fs on 2nd partition it boots and when the boot ends
    it starts an endless printout of:
    watchdog watchdog0: watchdog did not stop!

    if CONFIG_XILINX_FIXED_DEVTREE_ADDR is not set
    then booting the uImage with the on-ram fs is OK
    -
    but if I boot the zImage and the linaro fs on 2nd partition
    it generates the unrecognized/unsupported machine ID (r1=0x1fb6c62c)
    and says that the ID should be 00000d32
    -
    (I did configure the #define CONFIG_MACH_TYPE 0xd32 in u-boot,
    but this doesn't work)
    -
    when I compile the kernel with option:
    make ARCH=arm digilent_zed_defconfig
    -
    if CONFIG_XILINX_FIXED_DEVTREE_ADDR=y
    then booting the uImage with the on-ram fs hangs after writing:
    Uncompressing Linux... done, booting the kernel.
    -
    booting the zImage and the linaro fs on 2nd partition
    it starts an endless printout of:
    [  ss.cc0000]watchdog watchdog0: watchdog did not stop!
    if CONFIG_XILINX_FIXED_DEVTREE_ADDR is not set
    then booting the uImage with the on-ram fs is OK
    -
    if I boot the zImage and the linaro fs on 2nd partition it hangs after writing:
    Uncompressing Linux... done, booting the kernel.
    -
    in conclusion Linaro (or a FS from the 2nd partition) is usable only with the zImage from linux-3.3
    -
    how to fix the watchdog problem?
    it is very complicated to use the FS on ram and loosing everything at each turn-off
    I even tried to use linux-digilent-dev-3.8, with the same results;
    anyway within that Makefile there is the old 3.6.0 indication