Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Android on Zynq
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 30 replies
  • Subscribers 364 subscribers
  • Views 3042 views
  • Users 0 members are here
Related

Android on Zynq

shakith
shakith over 14 years ago

Hi all,

Is the android sources for Zynq out? Where can i download it from?

Cheers
Shakith

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    With the Digilent Linux kernel (https://github.com/Digilent/linux-3.3-digilent.git) and with the iveia Android sources (http://wiki.xilinx.com/android-on-zynq-building-bsp) I've actually succeeded booting into an Android system. Keyboard and mouse input does not work yet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I've created a basic documentation about building Android for ZedBoard. Is there a wiki or a site where I can upload it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Wachag,

    It would be really helpful if you could share the document with me.
    email: akini@synapticon.com

    Or, you could share a public link through DropBox or Google Drive.

    Thanks,
    Anup.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I have Android 2.3.7 running with VGA output and keyboard working. Currently trying to get 4.2.2 up.
    I've classes tomorrow, but I can try and publish the source (already going home for today :).

    Meanwhile, if you wanna give it a try, basically what I did was the following:

    1) Checked out the 3.3 kernel from Digilent.
    2) Checked out the 3.3 kernel from Google.
    3) Merged Google into Digilent.
    4) Created a new bitstream with the Xillybus VGA IP used in the Xillinux distribution, and generated a new boot.bin. Also manually modified the dts and generated a new blob.
    5) Merged the Xillybus VGA IP driver.
    6) Reconfigured the kernel, adding the android options (except the tracer) and the Xillybus driver. Note that the ipv6 support as module is broken, add it as built-in or remove it.

    That's it for the Linux kernel.

    For Android:
    1) I checked out the sources from Iveia. It did not compile at first so I had to do some quickfixes, nothing extraordinary though. Used generic-eng as lunch.
    2) At this point Android boots but the keyboard doesn't work. Kinda. It actually does, but the screen state (logically) seems to always stay locked, so the keyboard events end up never being sent to the application and it looks like it doesn't. There's an option in one of the .xml files so it never locks, or you can quickfix by short circuiting the test in Android's code. You may also want to change the keyboard layout, look for .kl files.

    I couldn't find support for the mouse and ethernet in the Iveia source, but I've found some patches from the androidX86 project to add them. Haven't tested it though. Anyway, adding them should be straightforward.
    Ethernet works ok in Linux and you can use adb without problems.

    Hope it helps :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    > Merged the Xillybus VGA IP driver.

    I've searched the Internet but could not find the Linux kernel driver for XillyVGA. Could you please tell where can you download it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I can't seem to use adb while i'm in Android on the ZedBoard:
    ---
    # adb
    adb: not found
    ---
    Also I can't seem to find the ethernet and mouse patches in de androidX86 project. Can you help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I can't seem to use adb while i'm in Android on the ZedBoard:
    ---
    # adb
    adb: not found
    ---
    Also I can't seem to find the ethernet and mouse patches in de androidX86 project. Can you help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    apparently "adb" is not available in the Android Shell, it's called "pm".