Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Writing Data From PL to DDR RAM problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 808 views
  • Users 0 members are here
Related

Writing Data From PL to DDR RAM problem

e14 Contributor
e14 Contributor over 10 years ago

I am working on data transferring from PL to DDR RAM. When I run the software application using JTAG, I could read and write to DDR from PS. But the data I write to DDR from my AXI DMA ,does not write on the DDR when my application is running. But after I stopped the application and re-run the application without switching off the board, the data is written on the DDR RAM. My guess is the problem is in my main() function. I may not be calling all the functions to configure the hardware platform correctly. But I can not figure out what it is. This is a sketch of my main() function and headers included in the program.  I am using SDK 2016.1 and Vivado 2016.1 for my design.

#include <stdio.h>
#include "platform.h"
#include "ps7_init.h"
#include "xil_printf.h"
#include "xil_io.h"
#include "xscugic.h"
#include "xparameters.h"
#include "xgpio.h"
 
int main()
{
     // Initializing hardware platform
     xil_printf("Initializing Hardware platform.....\n\r");
     init_platform();
 
     // ps7_post_config() to enable the level shifters @PS-PL boundary and release the RESET signal to enable the PL
 
     ps7_post_config();
 
     /******* program body ********/
     
     // DMA initialization
     //Interrupt initialization
     //GPIO initialization
 
     // infinite loop
     while(1){
          .
          . 
          .     
     }
     /******* end of body ********/
    cleanup_platform();
    return 0;
}
 
I am stuck here for few days now. But still could not find the solution. Hope some can resolve this issue. Thanks in advance..
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Hbmdds,

    Try taking a look at this forum post, it has a lot of excellent information in regards to PL accessing DDR.

    http://zedboard.org/content/how-access-data-ddr-ps-side-pl-part 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Thank you for the reply JFoster.

    Anyway, I figured the problem my self. It worked when I flushed the cash and read...