Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development boot.bin file from Yocto doesn't seem to work
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 1190 views
  • Users 0 members are here
Related

boot.bin file from Yocto doesn't seem to work

e14 Contributor
e14 Contributor over 10 years ago

Hi
I am new with the embedded software on Zynq and I am currently trying to boot Linux Kernel on Picozed Board from SD CARD.

I have followed some tutorial but the board doesn't boot with the boot.bin (38 528 bytes)

U-Boot SPL 2015.01 (Sep 07 2016 - 12:37:43)
Unsupported boot mode selected
### ERROR ### Please RESET the board ###

But I have no issue with the boot.bin from recovery image from Xillinx (6 358 716 bytes)...

I have missed something in Yocto?

Thanks for helping,

Regards,

-Trigger

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Trigger, 

    Please tell me which tutorial you are working through, it will help me to better guide you to a solution.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Josh,

    I have used this one : http://architechboards-picozed.readthedocs.io/en/latest/

    Everything seems to be fine in Yocto because I have the correct output files.

    Thanks,

    -Trigger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hi Trigger,

    You could be missing you PL bitstream in your Boot.bin file, however this may not be requried in your project. I am not familiar enough with that design to know if it is required. 

    Another option for support would be reaching out to those who created this design at http://architechboards.org/ 

    Another resource at your disposal would be the xilinx forum. https://forums.xilinx.com/ 

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi JFoster,

    I have some new conformations : I have now a a u-boot prompt :)

    I have build u-boot like that :

    cd ~/Documents
    git clone git://github.com/Xilinx/u-boot-xlnx.git
    cd u-boot-xlnx
    git checkout 58359ed54834e42e5f9ee336a7daa62c3c86c32a
    patch -p1 < ~/yocto/meta-xilinx/recipes-bsp/u-boot/u-boot-xlnx/zynq-Add-Zynq-PicoZed-board-support.patch
    patch -p1 < ~/yocto/meta-xilinx/recipes-bsp/u-boot/u-boot-xlnx/microblaze-Fix-EMAC-Lite-initialization.patch
    patch -p1 < ~/yocto/meta-xilinx/recipes-bsp/u-boot/u-boot-xlnx/microblaze-generic_defconfig-Disable-configs.patch

     

    With the SDK I have created a Boot.bin with

    1. FSBL.elf

    2. empty bitstream

    3. u-boot.elf

     

    But I think there is some trouble with Sd card communication because I have this error :

    sdhci_send_command: MMC: 0 busy timeout increasing to: 200 ms.
    sdhci_send_command: MMC: 0 busy timeout increasing to: 400 ms.
    sdhci_send_command: MMC: 0 busy timeout increasing to: 800 ms.
    sdhci_send_command: MMC: 0 busy timeout increasing to: 1600 ms.
    sdhci_send_command: MMC: 0 busy timeout increasing to: 3200 ms.
    sdhci_send_command: MMC: 0 busy timeout.
    ** Bad device mmc 0 **

    I tried to rebuild a FSBL after read this thread : https://forums.xilinx.com/t5/Embedded-Linux/Kernel-Boot-Failing-on-Zynq-in-U-Boot/td-p/703136

    Do you know if I need to copy ps7_init_gpl.c/h from hw project in u-boot sources ?

    But it's doesn't work :/

    Thank you for reading :)

    Any suggestion is welcome (or advice, help, suggestion, tricks or anything else)

     

    Regards,

    -Trigger