Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Enabling UART 0
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 363 subscribers
  • Views 2663 views
  • Users 0 members are here
Related

Enabling UART 0

e14 Contributor
e14 Contributor over 13 years ago

Dear all,

I'm trying to use the UART 0 peripheral on the Zedboard (I want to have two UARTs).

I have a very simple baremetal "hello world" that works when I use UART 1 (0xe0001000) but it doesn't when I use the UART 0 (0xe0000000).

So far, I managed to collect information about the pin mapping (see details later).

The main program of my hello world consists of the following steps:

#define SLCR_UNLOCK   0xF8000008
#define SLCR_LOCK     0xF8000004
#define APER_CLK_CTRL 0xF800012C
#define UART_CLK_CTRL 0xF8000154
#define MIO_PIN_10    0xF8000728
#define MIO_PIN_11    0xF800072C

#define REG(x) (*((volatile unsigned int *)(x)))

void main(void)
{
    REG(SLCR_UNLOCK) = 0xDF0D; // enable write
    REG(APER_CLK_CTRL) = REG(APER_CLK_CTRL) | 0x00100000;
    REG(UART_CLK_CTRL) = REG(UART_CLK_CTRL) | 0x1;
    REG(MIO_PIN_10) = 0x16E1; // [TRI_ENABLE=1 PULLUP=1, IO_Type=011(LVCMOS33=3.3V), L3_SEL=111(UART 0 RxD, Input)
    REG(MIO_PIN_11) = 0x16E0; // [TRI_ENABLE=0 PULLUP=1, IO_Type=011(LVCMOS33=3.3V), L3_SEL=111(UART 0 TxD, Output)
    REG(SLCR_LOCK) = 0x767B; // disable write

    uart_init();
    uart_puts("
Hello World
r");

    while(1);
}

Unfortunately, I'm not getting any output message.

I also tried using XPS to generate the same system (UART 0 mapped to MIO 10..11) and created a BSP. On the BSP the initialization value had PULLUP=0. I tried with that value but it also failed. (Note: I don't want to use MIO14..15 because my USB-serial cable is designed for 3.3V operation).

Can somebody indicate me what else should I do to make UART 0 working?

Thanks in advance,
Daniel

>>--------- Collected Pin-MMIO information -------<<

UART <=> MIO
============

http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

UART0 => rx=MIO-10 tx=MIO-11  or  rx=MIO-14 tx=MIO-15

PMOD pin <=> ZYNQ pin
=====================

http://www.zedboard.org/sites/default/files/documentations/ZedBoard_HW_UG_v1_9.pdf

Pmod | Signal Name | Zynq pin |
JE1       JE1          A6
MIO       JE2          G7
Pmod      JE3          B4
          JE4          C5
          JE7          G6
          JE8          C4
          JE9          B6
          JE10         E6

ZYNQ Pin <=> MIO pin
====================

http://www.xilinx.com/support/packagefiles/z7packages/xc7z020clg484pkg.txt

Pin   Pin Name                 Memory Byte Group  Bank  VCCAUX Group  Super Logic Region  I/O Type  No-Connect
A6    PS_MIO13_500             NA                 500   NA            NA                  MIO       NA
C5    PS_MIO12_500             NA                 500   NA            NA                  MIO       NA
B4    PS_MIO11_500             NA                 500   NA            NA                  MIO       NA
G7    PS_MIO10_500             NA                 500   NA            NA                  MIO       NA
C4    PS_MIO9_500              NA                 500   NA            NA                  MIO       NA
E5    PS_MIO8_500              NA                 500   NA            NA                  MIO       NA
D5    PS_MIO7_500              NA                 500   NA            NA                  MIO       NA
A4    PS_MIO6_500              NA                 500   NA            NA                  MIO       NA
A3    PS_MIO5_500              NA                 500   NA            NA                  MIO       NA
E4    PS_MIO4_500              NA                 500   NA            NA                  MIO       NA
F6    PS_MIO3_500              NA                 500   NA            NA                  MIO       NA
A2    PS_MIO2_500              NA                 500   NA            NA                  MIO       NA
A1    PS_MIO1_500              NA                 500   NA            NA                  MIO       NA
G6    PS_MIO0_500              NA                 500   NA            NA                  MIO       NA

My USB-Serial
=============

Olimex USB-Serial:
https://www.olimex.com/Products/Components/Cables/USB-Serial-Cable/USB-Serial-Cable-F/
[GND_usb] = Blue  => GND
[TXD_usb] = Red   => JE2
[RXD_usb] = Green => JE3

MIO configuration
=================

UART0
REG(MIO_PIN_10=0xF8000728) = 0x16E1 [TRI_ENABLE=1 PULLUP=1, IO_Type=011(LVCMOS33=3.3V), L3_SEL=111(UART 0 RxD, Input)
REG(MIO_PIN_11=0xF800072C) = 0x16E0 [TRI_ENABLE=0 PULLUP=1, IO_Type=011(LVCMOS33=3.3V), L3_SEL=111(UART 0 TxD, Output)


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'm not sure what you mean. What I can explain is how I managed to use the UART1.

    The hardware connections between the board and the USB cable are like i show above:

    [GND_usb] = Blue => GND
    [TXD_usb] = Red => JE2
    [RXD_usb] = Green => JE3

    (You can see a picture of the connections in the file
    safeg-1.0/doc/en/target/zynq/IMAG1048.jpg at
    http://www.toppers.jp/download.cgi/safeg-1.0.tar.gz)

    About the software please check the file:
    fmp/target/zynq_gcc/target_serial.c
    from
    http://www.toppers.jp/download.cgi/fmp_zynq_gcc-20131203.tar.gz

    Regards
    Daniel




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Sorry for my bad english and Thanks for answering me.

    I want to implement and OR1200 processor in addition to the existing ARM core. What I want to do is to somehow see the messages come from the OR1200 and also be able to send message to this core through UART.

    I think what you have done is using the PL(or PS) pins to connect the board to another UART device, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Sorry for my bad english and Thanks for answering me.

    I want to implement and OR1200 processor in addition to the existing ARM core. What I want to do is to somehow see the messages come from the OR1200 and also be able to send message to this core through UART.

    I think what you have done is using the PL(or PS) pins to connect the board to another UART device, right?