Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux OS with Custom Programmable Logic
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 335 views
  • Users 0 members are here
Related

Linux OS with Custom Programmable Logic

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I have modified the BOOT.bin file on the SD card to use my own FSBL, .bit file, and the u-boot.elf.  The problem with this is that when the default Linux image boots it looks for GPIO which isn't there and as a result it fails.  Is this a problem with the ramdisk or device tree, and if so how could I fix it?  If it's not a problem with these how can I get a Linux OS running on the ARM cores with my own logic design?

Thanks,
Matthew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Thanks for your response, I managed to get it working eventually.

    Turns out it wasn't the GPIO itself, the processor was trying to reset an AXI connector which I had replaced.  There seems to be very little documentation from Xilinx about the device tree, which is annoying since it looks quite important.  Fortunately the Tree Generator (http://wiki.xilinx.com/device-tree-generator), whilst not perfect [the Ethernet connection needed fixing], gave me a start.  Do you have any links which would be useful to learn more about how these work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Thanks for your response, I managed to get it working eventually.

    Turns out it wasn't the GPIO itself, the processor was trying to reset an AXI connector which I had replaced.  There seems to be very little documentation from Xilinx about the device tree, which is annoying since it looks quite important.  Fortunately the Tree Generator (http://wiki.xilinx.com/device-tree-generator), whilst not perfect [the Ethernet connection needed fixing], gave me a start.  Do you have any links which would be useful to learn more about how these work?