Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Kernel error while booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 429 views
  • Users 0 members are here
Related

Kernel error while booting

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I'm experiencing one problem with booting original Xillybus on my new Zedboard.
From time to time I get kernel error while booting process.
Could you please help identify the cause of this error?


Here's the listing:

root@localhost:~# shutdown -r now
root@localhost:~#
Broadcast message from root@localhost.localdomain
(/dev/ttyPS0) at 18:47 ...

The system is going down for reboot NOW!
Checking for running unattended-upgrades:
speech-dispatcher disabled; edit /etc/default/speech-dispatcher
* Asking all remaining processes to terminate... nm-dispatcher.action: Caught signal 15, shutting down...
nm-dispatcher.action: Script '/etc/NetworkManager/dispatcher.d/01ifupdown' exited abnormally.
[ OK ]
* All processes ended within 1 seconds.... [ OK ]
nm-dispatcher.action: Caught signal 15, shutting down...
modem-manager[1106]: <info> Caught signal 15, shutting down...

* Deconfiguring network interfaces... [ OK ]
* Deactivating swap... [ OK ]
/proc/misc: No entry for device-mapper found
Is device-mapper driver missing from kernel?
Failure to communicate with kernel device-mapper driver.
Command failed
/proc/misc: No entry for device-mapper found
Is device-mapper driver missing from kernel?
Failure to communicate with kernel device-mapper driver.
Command failed
umount: /run/lock: not mounted
* Will now restart
u2265 39.841077] reboot: Restarting system

U-Boot 2013.07-00003-g19ab76d (Apr 07 2014 - 03:02:52)

Memory: ECC disabled
DRAM: 512 MiB
MMC: zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
Net: Gem.e000b000
Hit any key to stop autoboot: 0
Device: zynq_sdhci
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
Booting Xillinux...
reading xillydemo.bit
4045675 bytes read in 301 ms (12.8 MiB/s)
design filename = "xillydemo.ncd;HW_TIMEOUT=FALSE;UserID=0xFFFFFFFF"
part number = "7z020clg484"
date = "2014/04/07"
time = "09:23:15"
bytes in bitstream = 4045564
zynq_load: Align buffer at 10006f to 100080(swap 1)
reading uImage
3647232 bytes read in 274 ms (12.7 MiB/s)
reading devicetree.dtb
8405 bytes read in 17 ms (482.4 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
Image Name: Linux-3.12.0-xillinux-1.3+
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3647168 Bytes = 3.5 MiB
Load Address: 00008000
Entry Point: 00008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
Booting using the fdt blob at 0x2a00000
Loading Kernel Image ... OK
Loading Device Tree to 1fb4e000, end 1fb530d4 ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Error: unrecognized/unsupported processor variant (0x413fc090).


--------------------------------------------------------------


root@localhost:~# reboot
root@localhost:~#
Broadcast message from root@localhost.localdomain
        (/dev/ttyPS0) at 0:00 ...

The system is going down for reboot NOW!
Checking for running unattended-upgrades:
speech-dispatcher disabled; edit /etc/default/speech-dispatcher
* Asking all remaining processes to terminate...                        [ OK ]
* All processes ended within 1 seconds....                              [ OK ]
* Deconfiguring network interfaces...                                   [ OK ]
* Deactivating swap...                                                  [ OK ]
/proc/misc: No entry for device-mapper found
Is device-mapper driver missing from kernel?
Failure to communicate with kernel device-mapper driver.
Command failed
/proc/misc: No entry for device-mapper found
Is device-mapper driver missing from kernel?
Failure to communicate with kernel device-mapper driver.
Command failed
umount: /run/lock: not mounted
* Will now restart
u2518   15.051739] reboot: Restarting system

U-Boot 2013.07 (Mar 15 2014 - 22:59:21)

Memory: ECC disabled
DRAM:  512 MiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL256S_64K with page size 64 KiB, total 32 MiB
*** Warning - bad CRC, using default environment

In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5344
Name: SL08G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 7.4 GiB
Bus Width: 4-bit
Booting Xillinux...
reading xillydemo.bit
4045675 bytes read in 295 ms (13.1 MiB/s)
  design filename = "xillydemo.ncd;HW_TIMEOUT=FALSE;UserID=0xFFFFFFFF"
  part number = "7z020clg484"
  date = "2014/04/13"
  time = "22:33:35"
  bytes in bitstream = 4045564
zynq_load: Align buffer at 10006f to 100080(swap 1)
reading uImage
3499448 bytes read in 258 ms (12.9 MiB/s)
reading devicetree.dtb
8109 bytes read in 15 ms (527.3 KiB/s)
## Booting kernel from Legacy Image at 03000000 ...
   Image Name:   Linux-3.12.0-xillinux-1.3
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3499384 Bytes = 3.3 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02a00000
   Booting using the fdt blob at 0x2a00000
   Loading Kernel Image ... OK
   Loading Device Tree to 1fb4e000, end 1fb52fac ... OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 3.12.0-xillinux-1.3 (eli@ocho.localdomain) (gcc version 4.5.1 (Sourcery G++ Lite 2010.09-62) ) #1 SMP PREEMPT Thu Mar 13 18:39:32 IST 2014
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] PERCPU: Embedded 7 pages/cpu @c0af8000 s7936 r8192 d12544 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
[    0.000000] Kernel command line: console=ttyPS0,115200n8 consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] allocated 1048576 bytes of page_cgroup
[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups
[    0.000000] Memory: 511536K/524288K available (4631K kernel code, 296K rwdata, 1744K rodata, 199K init, 200K bss, 12752K reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0641e24   (6376 kB)
[    0.000000]       .init : 0xc0642000 - 0xc0673f00   ( 200 kB)
[    0.000000]       .data : 0xc0674000 - 0xc06be3c0   ( 297 kB)
[    0.000000]        .bss : 0xc06be3cc - 0xc06f065c   ( 201 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Dump stacks of tasks blocking RCU-preempt GP.
[    0.000000]  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] ps7-slcr mapped to e0802000
[    0.000000] Zynq clock init
[    0.000000] sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207ms
[    0.000000] ps7-ttc #0 at e0804000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.008663] Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
[    0.094833] pid_max: default: 32768 minimum: 301
[    0.097008] Mount-cache hash table entries: 512
[    0.103496] Initializing cgroup subsys memory
[    0.105837] Initializing cgroup subsys devices
[    0.110224] Initializing cgroup subsys freezer
[    0.114703] Initializing cgroup subsys blkio
[    0.119016] Initializing cgroup subsys perf_event
[    0.123808] CPU: Testing write buffer coherency: ok
[    0.128914] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.134352] Setting up static identity map for 0xc045ffb0 - 0xc0460008
[    0.141024] L310 cache controller enabled
[    0.144913] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 512 kB
[    0.205573] CPU1: Booted secondary processor
[    0.294803] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.294932] Brought up 2 CPUs
[    0.302416] SMP: Total of 2 processors activated.
[    0.307171] CPU: All CPU(s) started in SVC mode.
[    0.312388] devtmpfs: initialized
[    0.317567] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.323853] regulator-dummy: no parameters
[    0.327484] NET: Registered protocol family 16
[    0.332737] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.343335] zynq_gpio e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe0850000
[    0.350155] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.353676] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.359648] zynq_ocm f800c000.ps7-ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0880000
[    0.395222] bio: create slab <bio-0> at 0
[    0.396844] vgaarb: loaded
[    0.397526] SCSI subsystem initialized
[    0.401010] usbcore: registered new interface driver usbfs
[    0.406005] usbcore: registered new interface driver hub
[    0.411332] usbcore: registered new device driver usb
[    0.416806] media: Linux media interface: v0.10
[    0.420916] Linux video capture interface: v2.00
[    0.426004] pps_core: LinuxPPS API ver. 1 registered
[    0.430409] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.439828] PTP clock support registered
[    0.443827] EDAC MC: Ver: 3.0.0
[    0.447809] Advanced Linux Sound Architecture Driver Initialized.
[    0.453836] Switched to clocksource ttc_clocksource
[    0.475531] NET: Registered protocol family 2
[    0.476194] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[    0.481595] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
[    0.488194] TCP: Hash tables configured (established 4096 bind 4096)
[    0.494368] TCP: reno registered
[    0.497576] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.503437] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.510552] NET: Registered protocol family 1
[    0.514423] RPC: Registered named UNIX socket transport module.
[    0.520008] RPC: Registered udp transport module.
[    0.524782] RPC: Registered tcp transport module.
[    0.529482] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.536431] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.547011] VFS: Disk quotas dquot_6.5.2
[    0.548098] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.555195] NFS: Registering the id_resolver key type
[    0.559618] Key type id_resolver registered
[    0.563784] Key type id_legacy registered
[    0.567894] jffs2: version 2.2. (NAND) (SUMMARY)  u252Cu2310 2001-2006 Red Hat, Inc.
[    0.575101] msgmni has been set to 999
[    0.579451] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 249)
[    0.586216] io scheduler noop registered
[    0.590013] io scheduler deadline registered
[    0.594363] io scheduler cfq registered (default)
[    1.496083] Console: switching to colour frame buffer device 128x48
[    1.524947] e0001000.serial: ttyPS0 at[    1.528560] console [ttyPS0] enabled, bootconsole disabled
[    1.528560] console [ttyPS0] enabled, bootconsole disabled
[    1.534753] xdevcfg f8007000.ps7-dev-cfg: ioremap 0xf8007000 to e0864000
[    1.557812] brd: module loaded
[    1.566457] loop: module loaded
[    1.577166] xqspips e000d000.ps7-qspi: master is unqueued, this is deprecated
[    1.584797] m25p80 spi0.0: found s25fl256s1, expected n25q128
[    1.590547] m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
[    1.595487] 5 ofpart partitions found on MTD device spi0.0
[    1.600906] Creating 5 MTD partitions on "spi0.0":
[    1.605717] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    1.612777] 0x000000100000-0x000000600000 : "qspi-linux"
[    1.619633] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    1.626601] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    1.633107] 0x000000c00000-0x000001000000 : "qspi-bitstream"
[    1.639964] xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xE0866000, irq=51
[    1.649825] libphy: Fixed MDIO Bus: probed
[    1.655724] libphy: XEMACPS mii bus: probed
[    1.660608] xemacps e000b000.ps7-ethernet: pdev->id -1, baseaddr 0xe000b000, irq 54
[    1.668681] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.675354] ehci-pci: EHCI PCI platform driver
[    1.680128] ULPI transceiver vendor/product ID 0x0451/0x1507
[    1.685731] Found TI TUSB1210 ULPI transceiver.
[    1.690229] ULPI integrity check: passed.
[    1.694486] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    1.701214] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    1.733894] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    1.753875] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    1.760805] hub 1-0:1.0: USB hub found
[    1.764529] hub 1-0:1.0: 1 port detected
[    1.769026] usbcore: registered new interface driver usb-storage
[    1.775828] mousedev: PS/2 mouse device common for all mice
[    1.781910] i2c /dev entries driver
[    1.786186] IR NEC protocol handler initialized
[    1.790629] IR RC5(x) protocol handler initialized
[    1.795439] IR RC6 protocol handler initialized
[    1.799918] IR JVC protocol handler initialized
[    1.804490] IR Sony protocol handler initialized
[    1.809042] IR RC5 (streamzap) protocol handler initialized
[    1.814609] IR SANYO protocol handler initialized
[    1.819272] IR MCE Keyboard/mouse protocol handler initialized
[    1.825981] xadcps f8007100.ps7-xadc: enabled:       yes     reference:      external
[    1.833004] zynq-edac f8006000.ps7-ddrc: ecc not enabled
[    1.838589] sdhci: Secure Digital Host Controller Interface driver
[    1.844709] sdhci: Copyright(c) Pierre Ossman
[    1.849022] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.854828] mmc0: no vqmmc regulator found
[    1.858828] mmc0: no vmmc regulator found
[    1.893886] mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA
[    1.907065] usbcore: registered new interface driver usbhid
[    1.912576] usbhid: USB HID core driver
[    1.921349] pmodoled-gpio-spi [zed_oled] SPI Probing
[    1.965513] mmc0: new high speed SDHC card at address aaaa
[    1.971319] mmcblk0: mmc0:aaaa SL08G 7.40 GiB
[    1.977051]  mmcblk0: p1 p2
[    2.099662] no UART detected at 0x1
[    2.104326] TCP: cubic registered
[    2.107588] NET: Registered protocol family 15
[    2.112085] Key type dns_resolver registered
[    2.116546] Registering SWP/SWPB emulation handler
[    2.122039] registered taskstats version 1
[    2.126481] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    2.136176] ALSA device list:
[    2.139052]   No soundcards found.
[    2.143623] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[    2.152194] EXT4-fs (mmcblk0p2): couldn't mount as ext2 due to feature incompatibilities
[    2.177483] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.185538] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.194293] devtmpfs: mounted
[    2.197445] Freeing unused kernel memory: 196K (c0642000 - c0673000)
[    2.222457] Unable to handle kernel NULL pointer dereference at virtual address 00000001
[    2.230475] pgd = c0004000
[    2.233148] [00000001] *pgd=00000000
[    2.236724] Internal error: Oops: 805 [#1] PREEMPT SMP ARM
[    2.242180] Modules linked in:
[    2.245221] CPU: 0 PID: 674 Comm: mmcqd/0 Not tainted 3.12.0-xillinux-1.3 #1
[    2.252262] task: df6836c0 ti: df75a000 task.ti: df75a000
[    2.257644] PC is at _set_bit+0x4/0x50
[    2.261368] LR is at mpage_end_io+0x74/0xcc
[    2.265533] pc : [<c01eb654>]    lr : [<c00f5548>]    psr: 20000113
[    2.265533] sp : df75be50  ip : 00000001  fp : 00000000
[    2.276998] r10: 00000000  r9 : 00000000  r8 : 00004000
[    2.282196] r7 : 00000001  r6 : defcb478  r5 : 00000001  r4 : c0af2660
[    2.288702] r3 : c0af2670  r2 : 00000000  r1 : 00000001  r0 : 00000003
[    2.295227] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment kernel
[    2.302508] Control: 18c5387d  Table: 0000404a  DAC: 00000015
[    2.308241] Process mmcqd/0 (pid: 674, stack limit = 0xdf75a240)
[    2.314231] Stack: (0xdf75be50 to 0xdf75c000)
[    2.318563] be40:                                     defcb440 00000000 00004000 defcb440
[    2.326728] be60: 00004000 c00eddc0 122c8000 df792348 00000000 c01d615c df792348 00000000
[    2.334893] be80: df792348 00000000 00000000 df5f7250 df74bc00 df5f7000 df792348 c01d62ec
[    2.343059] bea0: defd5a68 df792348 00000000 c01d6358 00000000 df5f7008 df5f7148 df5f7250
[    2.351206] bec0: df74bc00 c0356cc0 df792348 df6e5970 00000000 00000000 00000000 df5f714c
[    2.359371] bee0: 00000000 00000000 df6836c0 00000000 00100100 00000000 df74bc00 df5f42c8
[    2.367537] bf00: df5f7008 df5f4000 00000000 df5f7000 00000000 c03574fc df5f7008 00000000
[    2.375684] bf20: 00000000 df5f7008 df5f7010 defd5a68 00000000 00000000 00000000 df792348
[    2.383849] bf40: 00000000 c0357d2c 00000000 df47dd24 00000000 df5f7008 c0357c74 00000000
[    2.392015] bf60: 00000000 c003a9c0 df62f238 00000000 00000000 df5f7008 00000000 00000000
[    2.400162] bf80: df75bf80 df75bf80 00000000 00000000 df75bf90 df75bf90 df75bfac df47dd24
[    2.408327] bfa0: c003a920 00000000 00000000 c000dbf8 00000000 00000000 00000000 00000000
[    2.416474] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[    2.424640] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000 df75bff8 df75bff8
[    2.432823] [<c01eb654>] (_set_bit+0x4/0x50) from [<c00f5548>] (mpage_end_io+0x74/0xcc)
[    2.440805] [<c00f5548>] (mpage_end_io+0x74/0xcc) from [<c00eddc0>] (bio_endio+0x48/0x4c)
[    2.448952] [<c00eddc0>] (bio_endio+0x48/0x4c) from [<c01d615c>] (blk_update_request+0x23c/0x3b8)
[    2.457817] [<c01d615c>] (blk_update_request+0x23c/0x3b8) from [<c01d62ec>] (blk_update_bidi_request+0x14/0x6c)
[    2.467881] [<c01d62ec>] (blk_update_bidi_request+0x14/0x6c) from [<c01d6358>] (blk_end_bidi_request+0x14/0x50)
[    2.477945] [<c01d6358>] (blk_end_bidi_request+0x14/0x50) from [<c0356cc0>] (mmc_blk_issue_rw_rq+0x554/0x9d4)
[    2.487843] [<c0356cc0>] (mmc_blk_issue_rw_rq+0x554/0x9d4) from [<c03574fc>] (mmc_blk_issue_rq+0x3bc/0x418)
[    2.497557] [<c03574fc>] (mmc_blk_issue_rq+0x3bc/0x418) from [<c0357d2c>] (mmc_queue_thread+0xb8/0x138)
[    2.506939] [<c0357d2c>] (mmc_queue_thread+0xb8/0x138) from [<c003a9c0>] (kthread+0xa0/0xac)
[    2.515363] [<c003a9c0>] (kthread+0xa0/0xac) from [<c000dbf8>] (ret_from_fork+0x14/0x3c)
[    2.523418] Code: e1a0f00e e3e0000d e1a0f00e e211c003 (15cc1000)
[    2.529537] ---[ end trace 78f8d40321b9887a ]---


--------------------------------------------------------------


root@localhost:~# dmesg
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 3.12.0-xillinux-1.3 (eli@ocho.localdomain) (gcc version 4.5.1 (Sourcery G++ Lite 2010.09-62) ) #1 SMP PREEMPT Thu Mar 13 18:39:32 IST 2014
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] On node 0 totalpages: 131072
[    0.000000] free_area_init_node: node 0, pgdat c06bd740, node_mem_map c06f1000
[    0.000000]   Normal zone: 1024 pages used for memmap
[    0.000000]   Normal zone: 0 pages reserved
[    0.000000]   Normal zone: 131072 pages, LIFO batch:31
[    0.000000] PERCPU: Embedded 7 pages/cpu @c0af8000 s7936 r8192 d12544 u32768
[    0.000000] pcpu-alloc: s7936 r8192 d12544 u32768 alloc=8*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
[    0.000000] Kernel command line: console=ttyPS0,115200n8 consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] allocated 1048576 bytes of page_cgroup
[    0.000000] please try 'cgroup_disable=memory' option if you don't want memory cgroups
[    0.000000] Memory: 511536K/524288K available (4631K kernel code, 296K rwdata, 1744K rodata, 199K init, 200K bss, 12752K reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc0641e24   (6376 kB)
[    0.000000]       .init : 0xc0642000 - 0xc0673f00   ( 200 kB)
[    0.000000]       .data : 0xc0674000 - 0xc06be3c0   ( 297 kB)
[    0.000000]        .bss : 0xc06be3cc - 0xc06f065c   ( 201 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Dump stacks of tasks blocking RCU-preempt GP.
[    0.000000]  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] ps7-slcr mapped to e0802000
[    0.000000] Zynq clock init
[    0.000000] sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207ms
[    0.000000] ps7-ttc #0 at e0804000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.008644] Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
[    0.094833] pid_max: default: 32768 minimum: 301
[    0.097008] Mount-cache hash table entries: 512
[    0.103478] Initializing cgroup subsys memory
[    0.105837] Initializing cgroup subsys devices
[    0.110224] Initializing cgroup subsys freezer
[    0.114684] Initializing cgroup subsys blkio
[    0.119016] Initializing cgroup subsys perf_event
[    0.123808] CPU: Testing write buffer coherency: ok
[    0.128896] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.134333] Setting up static identity map for 0xc045ffb0 - 0xc0460008
[    0.141024] L310 cache controller enabled
[    0.144913] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 512 kB
[    0.205573] CPU1: Booted secondary processor
[    0.294803] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.294932] Brought up 2 CPUs
[    0.302434] SMP: Total of 2 processors activated.
[    0.307171] CPU: All CPU(s) started in SVC mode.
[    0.312388] devtmpfs: initialized
[    0.317567] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.323853] regulator-dummy: no parameters
[    0.327484] NET: Registered protocol family 16
[    0.332700] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.343335] zynq_gpio e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe0850000
[    0.350137] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.353694] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.359648] zynq_ocm f800c000.ps7-ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0880000
[    0.395646] bio: create slab <bio-0> at 0
[    0.396899] vgaarb: loaded
[    0.397600] SCSI subsystem initialized
[    0.401434] usbcore: registered new interface driver usbfs
[    0.406908] usbcore: registered new interface driver hub
[    0.411774] usbcore: registered new device driver usb
[    0.417211] media: Linux media interface: v0.10
[    0.421340] Linux video capture interface: v2.00
[    0.426335] pps_core: LinuxPPS API ver. 1 registered
[    0.430833] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.440123] PTP clock support registered
[    0.444270] EDAC MC: Ver: 3.0.0
[    0.448196] Advanced Linux Sound Architecture Driver Initialized.
[    0.454297] Switched to clocksource ttc_clocksource
[    0.476563] NET: Registered protocol family 2
[    0.477245] TCP established hash table entries: 4096 (order: 3, 32768 bytes)
[    0.482627] TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
[    0.489207] TCP: Hash tables configured (established 4096 bind 4096)
[    0.495438] TCP: reno registered
[    0.498608] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.504561] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.510957] NET: Registered protocol family 1
[    0.515473] RPC: Registered named UNIX socket transport module.
[    0.521058] RPC: Registered udp transport module.
[    0.525814] RPC: Registered tcp transport module.
[    0.530514] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.536984] PCI: CLS 0 bytes, default 64
[    0.537389] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.548135] VFS: Disk quotas dquot_6.5.2
[    0.549130] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.556245] NFS: Registering the id_resolver key type
[    0.560669] Key type id_resolver registered
[    0.564890] Key type id_legacy registered
[    0.568908] jffs2: version 2.2. (NAND) (SUMMARY)  xffffffc2xffffffa9 2001-2006 Red Hat, Inc.
[    0.576134] msgmni has been set to 999
[    0.580465] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 249)
[    0.587174] io scheduler noop registered
[    0.591064] io scheduler deadline registered
[    0.595395] io scheduler cfq registered (default)
[    1.497225] Console: switching to colour frame buffer device 128x48
[    1.526422] e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 82, base_baud = 3124999) is a xuartps
[    1.530035] console [ttyPS0] enabled, bootconsole disabled
[    1.536246] xdevcfg f8007000.ps7-dev-cfg: ioremap 0xf8007000 to e0864000
[    1.558697] brd: module loaded
[    1.567010] loop: module loaded
[    1.577811] xqspips e000d000.ps7-qspi: master is unqueued, this is deprecated
[    1.585479] m25p80 spi0.0: found s25fl256s1, expected n25q128
[    1.591229] m25p80 spi0.0: s25fl256s1 (32768 Kbytes)
[    1.596372] 5 ofpart partitions found on MTD device spi0.0
[    1.601773] Creating 5 MTD partitions on "spi0.0":
[    1.606583] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    1.613551] 0x000000100000-0x000000600000 : "qspi-linux"
[    1.619965] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    1.626877] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    1.633347] 0x000000c00000-0x000001000000 : "qspi-bitstream"
[    1.640167] xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xE0866000, irq=51
[    1.650010] libphy: Fixed MDIO Bus: probed
[    1.655945] libphy: XEMACPS mii bus: probed
[    1.660811] xemacps e000b000.ps7-ethernet: pdev->id -1, baseaddr 0xe000b000, irq 54
[    1.668921] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.675575] ehci-pci: EHCI PCI platform driver
[    1.680349] ULPI transceiver vendor/product ID 0x0451/0x1507
[    1.686045] Found TI TUSB1210 ULPI transceiver.
[    1.690487] ULPI integrity check: passed.
[    1.694744] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    1.701472] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    1.744327] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    1.764326] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    1.771275] hub 1-0:1.0: USB hub found
[    1.774980] hub 1-0:1.0: 1 port detected
[    1.779496] usbcore: registered new interface driver usb-storage
[    1.786297] mousedev: PS/2 mouse device common for all mice
[    1.792361] i2c /dev entries driver
[    1.796601] IR NEC protocol handler initialized
[    1.801043] IR RC5(x) protocol handler initialized
[    1.805854] IR RC6 protocol handler initialized
[    1.810333] IR JVC protocol handler initialized
[    1.814867] IR Sony protocol handler initialized
[    1.819438] IR RC5 (streamzap) protocol handler initialized
[    1.825023] IR SANYO protocol handler initialized
[    1.829686] IR MCE Keyboard/mouse protocol handler initialized
[    1.836377] xadcps f8007100.ps7-xadc: enabled:       yes     reference:      external
[    1.843418] zynq-edac f8006000.ps7-ddrc: ecc not enabled
[    1.849003] sdhci: Secure Digital Host Controller Interface driver
[    1.855123] sdhci: Copyright(c) Pierre Ossman
[    1.859436] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.866237] mmc0: no vqmmc regulator found
[    1.870256] mmc0: no vmmc regulator found
[    1.914327] mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA
[    1.927506] usbcore: registered new interface driver usbhid
[    1.933017] usbhid: USB HID core driver
[    1.939726] pmodoled-gpio-spi [zed_oled] SPI Probing
[    1.975024] mmc0: new high speed SDHC card at address 0007
[    1.980812] mmcblk0: mmc0:0007 SD04G 3.70 GiB
[    1.987226]  mmcblk0: p1 p2
[    2.120103] no UART detected at 0x1
[    2.124748] TCP: cubic registered
[    2.128011] NET: Registered protocol family 15
[    2.132471] Key type dns_resolver registered
[    2.136914] Registering SWP/SWPB emulation handler
[    2.142388] registered taskstats version 1
[    2.146849] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    2.156544] ALSA device list:
[    2.159419]   No soundcards found.
[    2.166147] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[    2.176690] EXT4-fs (mmcblk0p2): couldn't mount as ext2 due to feature incompatibilities
[    2.228429] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.236484] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.248723] devtmpfs: mounted
[    2.251875] Freeing unused kernel memory: 196K (c0642000 - c0673000)
[    4.386172] udevd[787]: starting version 175
[    5.486590] lp: driver loaded but no devices found
[    5.706854] xillybus_core: module is from the staging directory, the quality is unknown, you have been warned.
[    5.766538] ppdev: user-space parallel port driver
[    5.778887] xillybus_of: module is from the staging directory, the quality is unknown, you have been warned.
[    5.866366] NET: Registered protocol family 10
[    6.223066] xillybus_of 50000000.xillybus: Created 7 device files.
[    6.910751] init_stage2: failsafe main process (1228) killed by TERM signal
[    7.299780] NET: Registered protocol family 17
[   10.788804] init_stage2: atd main process (1410) terminated with status 1
[   10.788970] init_stage2: atd main process ended, respawning
root@localhost:~#

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'll cling to "from time to time". If the boot isn't repeatable, something's wrong with your hardware. Assuming that the board itself is OK, the immediate suspect is your SD card. You are using a Sandisk, right? If not, get yourself one. A variety of exotic problems have been solved by buying a proper flash card.

    Regards,
      Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I tried several different vendors of SD card include Sandisk.
    Error appears on all of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I can see that you're using your own U-boot binary. Since the processor's initialization is done by U-boot (or ps7_start.c, which is generated by XPS/SDK depending on the system's configuration), that could cause a faulty hardware setting.

    Please use Xillinux' U-boot (that is, boot.bin), and see if the problem remains.

    Regards,
       Eli