Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Using the amba bus on arm (embedded)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 616 views
  • Users 0 members are here
Related

Using the amba bus on arm (embedded)

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I ran the linux from the Zedboard itself, and there I'm writing code c for example to get data from the Ethernet.

Now I want to send this data I have got to the amba bus (in order to process this data in Vivado. I meant I want to send this data to the amba bus and to get it from the amba bus in Vivado(in Fpga).
My question is how do I do this in c?
How I send this data to the amba? Is there any library to work with the bus which have the function, for example : senddata(data) and ect.

Thank you very much.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    There is a lot of detail required to answer your questions. I suggest you first take a look at the Zynq Hardware Development and PetaLinux trainings available at http://zedboard.org/support/trainings-and-videos

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bhfletcher

    Hello,
    Thanks for your reply.
    I have scanned these trainings, but maybe I miss the point.
    I will explain my self.
    I have data in the ps section, I want to transfer this data to the pl section via the "amba" bus technology of "Arm", that's why I think that I don't need "petalinux". Fix me if I wrong.

    Maybe I waste my time? Like maybe I need to put some data in the memory on the ps section. And to read this data in the pl section? (And it works with the amab)
    And I shouldn't search for a library or source of functions to use the amba bus?

    Thanks and sorry for my English..
    Have a great day.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    When you create an AXI Lite connection in a hardware peripheral and connect it to the ARM processor through the GP ports it automatically assigns an address range to your peripheral.  If you are in standalone mode you can write directly to this address to write to your peripheral.  The ZynqGeek blog post on this is very old now, but it covers some of the basics which may be useful:

    http://zedboard.org/content/talking-custom-peripheral-bare-metal

    Matthew