Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PS_DMA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 730 views
  • Users 0 members are here
Related

PS_DMA

e14 Contributor
e14 Contributor over 13 years ago

Hello,

Iu2019m using PS_DMAC to transfer data. But the DMA Controller needs a lot of time to start the DMA transfer using u201CXDmaPs_Startu201D. Why did the DMA Controller need this long time even u201CXDmaPs_Startu201D was used for a different channel before? Is there a way to reduce this time for multiple DMA-transfers?

Thanks in advance

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    https://github.com/shakith/zedboard/blob/master/Documentation/DMA-API-HOWTO.txt
    This might help...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    particularly, this:
    "If you need to use the same streaming DMA region multiple times and touch
    the data in between the DMA transfers, the buffer needs to be synced
    properly in order for the cpu and device to see the most uptodate and
    correct copy of the DMA buffer."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello HarbingerZjC,

    Thanks for your reply. Iu2019m programming without Linux. Iu2019m not sure if I understand it right. The DMA uses a buffer to safe the source memory content before transferring it to destination memory. Right? Is this buffer meant?

    I measured 4,875u00B5s to safe 4Kbyte of data into PL over AXI. The DDR3-RAM is much faster, so I think that reading the Data from DDR3-RAM into the DMA_buffer have to be much faster than writing it from buffer into PL, but it takes 5 to 6 times as much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Is it possible to start two or more Channels in parallel, like it is described in ug585 TRM page 207.