Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development getchar()
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 818 views
  • Users 0 members are here
Related

getchar()

e14 Contributor
e14 Contributor over 11 years ago

I am trying to "echo" any input over the UART, back to the console, as it is entered.

So I am trying to use getchar(). However, when I step through it on the debugger, I see that I don't have anything in the buffer for getchat() to pull out, until I hit enter in the terminal. Then the buffer is full of everything I just typed, and getchar() will go through and pull them out one at a time.
However I know that my terminal is sending every character as I type it.

I have read on this forum that the UART has a buffer. Is it storing up my input until I hit enter, and thus preventing getchar() from getting it as I type it?

Any help would be really helpful. Is there maybe a way to disable the UART buffer? Or to flush it every time a character is received?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I think that getchar() waits for the 'enter' by design. You can use the inbyte() function to get each character as you type it.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thank you Gary, that was exactly what I was looking for. I only wish I could have found it while searching online.

    In case it helps someone at a later date, here is my code to echo input as it is written:
    void echo(void)
    {
    memset(command, '0', 64);//"reset" our holder string
    tint i = 0;
    tdo{
    tcommand[i] = inbyte();
    tprintf("%c", command[i]);
    tfflush(stdout);
    ti++;
    t}while(command[i-1] != 'r');//Our "command" will have a return character included at the end.
    tprintf("
    ");//But we still need a new line character (if we want one)
    }//It is possible to overwrite the null terminating character at the end of the string. Fix if needed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    meant
    putchar(command[i]);
    instead of
    printf("%c", command[i]);
    Waste not, want not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Now featuring 100% more backspace implementation:
    char command[64];//Can be any size, though out of bounds isn't checked for.
    void echo(void)
    {
    tmemset(command, '0', 64);
    tint i = 0;

    tdo{
    tcommand[i] = inbyte();
    tputchar(command[i]);
    tfflush(stdout);
    tif(command[i] == 'b')
    t{
    ttcommand[i] = '0';
    ttcommand[i-1] = '0';
    tti = (i-2);
    ttputchar(' ');
    ttputchar('b');
    ttfflush(stdout);
    ttif(i<-1){i=-1;}
    t}
    ti++;
    t}while(command[i-1] != 'r');
    tprintf("
    ");
    }