Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development uZed program download speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 635 views
  • Users 0 members are here
Related

uZed program download speed

edoreshef
edoreshef over 9 years ago

Hi everyone,

I'm using a FreeRTOS over uzed and everything works great. The only issue I have is long development cycle.

Large chunk of the time it takes to modify-build-program-download-run is the firmware download part.

Looking at the XSDB Console I get this:

xsdb% Info: tcfchan#1 closed
xsdb% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff20 (Hardware Breakpoint)
xsdb% Info: ARM Cortex-A9 MPCore #1 (target 3) Stopped at 0xffffff34 (Suspended)
100%    3MB   3.0MB/s  00:01   <= FPGA download speed
Downloading Program -- uzed_app.elf
section, .text: 0x00100000 - 0x003479d3
section, .init: 0x003479d4 - 0x003479eb
section, .fini: 0x003479ec - 0x00347a03
section, .rodata: 0x00347a10 - 0x003855b3
    ... about 1500 section lines 
section, .fini_array: 0x003adc28 - 0x003adc5b
section, .bss: 0x00400000 - 0x0060812f
section, .heap: 0x00608130 - 0x1060812f
section, .stack: 0x10608130 - 0x1080992f
100%    2MB   0.0MB/s  01:43    <= Program download speed
Setting PC to Program Start Address 0x00100000
Successfully downloaded uzed_app.elf 

This paste shows the FPGA programming speed is great but for some reason firmware programming speed is about 100 slower.

Questions:

  1.   Is it normal?
  2.   Why is there a differance between the FPGA download speed and the firmware download speed?
  3.   Is there anything I can do to improve this?

Best Regards,
Edo

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Edo,

    Sorry for taking so long to reply. 

    1&2: That is the extent of the knowledge I know of on that subject.

    3: As for having to SD card over every time. When I typically do development I maybe change the Firmware 2-3 times , so SD carding that data over to the development board is no issue for me. Then I use the JTAG interface to quickly program my developmnet board over and over again as I make changes. But I can see it being an issue if you are changing the firmware ever time.

    If you want to try and reach a broader audience, you could try posting this question over at the xilinx forum.

    https://forums.xilinx.com/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Edo,

    Sorry for taking so long to reply. 

    1&2: That is the extent of the knowledge I know of on that subject.

    3: As for having to SD card over every time. When I typically do development I maybe change the Firmware 2-3 times , so SD carding that data over to the development board is no issue for me. Then I use the JTAG interface to quickly program my developmnet board over and over again as I make changes. But I can see it being an issue if you are changing the firmware ever time.

    If you want to try and reach a broader audience, you could try posting this question over at the xilinx forum.

    https://forums.xilinx.com/

    --Josh