Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Getting no output on my CAN0 TX port
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 326 views
  • Users 0 members are here
Related

Getting no output on my CAN0 TX port

cuevas1208
cuevas1208 over 9 years ago

I have my CAN0 TX connected to an oscilloscope but I am getting no output on my CAN0 TX port when I do cansend (petalinux), Any Ideas? 

 

root@petalinux_testSPI:/# ip link set can0 type can bitrate 100000
xilinx_can e0008000.can can0: bitrate error 0.0%
root@petalinux_testSPI:/# ip link set can0 type can bitrate 200000
xilinx_can e0008000.can can0: bitrate error 0.3%
root@petalinux_testSPI:/# ip link set can0 up
root@petalinux_testSPI:/# cansend can0 -i 0x14 0x33 0x88
Usage: cansend <device> <can_frame>.
root@petalinux_testSPI:/# cansend can0 111#1122334455667788 
root@petalinux_testSPI:/# cat /proc/net/can/stats

        1 transmitted frames (TXF)
       18 received frames (RXF)
        0 matched frames (RXMF)

        0 % total match ratio (RXMR)
        0 frames/s total tx rate (TXR)
        0 frames/s total rx rate (RXR)

        0 % current match ratio (CRXMR)
        0 frames/s current tx rate (CTXR)
        0 frames/s current rx rate (CRXR)

        0 % max match ratio (MRXMR)
        1 frames/s max tx rate (MTXR)
       18 frames/s max rx rate (MRXR)

        0 current receive list entries (CRCV)
        0 maximum receive list entries (MRCV)

root@petalinux_testSPI:/# ifconfig can0
can0      Link encap:UNSPEC  HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00  
          UP NOARP  MTU:16  Metric:1
          RX packets:18 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:18 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:10 
          RX bytes:144 (144.0 B)  TX bytes:8 (8.0 B)
          Interrupt:22 

root@petalinux_testSPI:/# candump can0
^Croot@petalinux_testSPI:/# 
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello,

    What evaluation platform of ours are you using?

    --Josh