Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picozed SDR 2x2+vivado 2015.4.2 fbsl can't boot from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1186 views
  • Users 0 members are here
Related

picozed SDR 2x2+vivado 2015.4.2 fbsl can't boot from SD card

denglin12315
denglin12315 over 9 years ago
Hi,everyone
I am using "Picozed SDR 2x2" and "PicoZed SDR FMC Carrier Card AES-PZSDRCC-FMC-G" for my work.
 
But I am facing a problem now.I want to control a led on Carrier Card(connect to zynq pin A8) by the manner of use PS + AXT_GPIO.
 
first, I use vivado create hardware diagram,and export it to SDK,after that ,I use SDK create an application as the template of Memory_Test in SDK and I add my own code to contorl the Led. And then,I use JTAG program FPGA and debug Memory_Test,It all works.
 
After that,I use SDK create an application project as the template of Fbsl in SDK,and using bootgen tools in the SDK create a boot image named boot.bin. Copy boot.bin in a SD card and set boot from SD,the fbsl print some information as follows:
 
--------------------------------------------
Xilinx First Stage Boot Loader 
Release 2015.4  Dec 29 2016-09:33:54
Devcfg driver initialized 
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD Init Done 
Flash Base Address: 0xE0100000
Reboot status register: 0x60400000
Multiboot Register: 0x0000C000
Image Start Address: 0x00000000
Partition Header Offset:0x00000C80
Partition Count: 3
Partition Number: 1
Header Dump
Image Word Len: 0x0032D130
Data Word Len: 0x0032D130
Partition Word Len:0x0032D130
Load Addr: 0x00000000
Exec Addr: 0x00000000
Partition Start: 0x000065D0
Partition Attr: 0x00000020
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xFF67242E
Bitstream
In FsblHookBeforeBitstreamDload function 
PCAP:StatusReg = 0x40000A30
PCAP:device ready
PCAP:Clear done
Level Shifter Value = 0xA
Devcfg Status register = 0x40000A30
PCAP:Fabric is Initialized done
PCAP register dump:
PCAP CTRL 0xF8007000: 0x4C00E07F
PCAP LOCK 0xF8007004: 0x0000001A
PCAP CONFIG 0xF8007008: 0x00000508
PCAP ISR 0xF800700C: 0x0802000B
PCAP IMR 0xF8007010: 0xFFFFFFFF
PCAP STATUS 0xF8007014: 0x00003A30
PCAP DMA SRC ADDR 0xF8007018: 0x00100001
PCAP DMA DEST ADDR 0xF800701C: 0xFFFFFFFF
PCAP DMA SRC LEN 0xF8007020: 0x0032D130
PCAP DMA DEST LEN 0xF8007024: 0x0032D130
PCAP ROM SHADOW CTRL 0xF8007028: 0xFFFFFFFF
PCAP MBOOT 0xF800702C: 0x0000C000
PCAP SW ID 0xF8007030: 0x00000000
PCAP UNLOCK 0xF8007034: 0x757BDF0D
PCAP MCTRL 0xF8007080: 0x30800100
...................................................................................................
DMA Done ! 
 
FPGA Done ! 
In FsblHookAfterBitstreamDload function 
Partition Number: 2
Header Dump
Image Word Len: 0x00003003
Data Word Len: 0x00003003
Partition Word Len:0x00003003
Load Addr: 0x00000000
Exec Addr: 0x00000000
Partition Start: 0x00333700
Partition Attr: 0x00000010
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xFFCC3685
Application
Handoff Address: 0x00000000
In FsblHookBeforeHandoff function 
No Execution Address JTAG handof
 
 
 
My tool version is: vavido 2015.4.2.
Thanks.
 
 
 
  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi denglin12315,

    Hmmm, those are some interesting clues that you point out where some applications work but others do not.  I have seen that before where applications run from OCM work but running from DDR does not.  This led me to tracking the problem down to a bad DDR configuration from Vivado.  I don't think that is the case here because if you are able to run Memory_Test successfully, then that indicates that DDR memory has been configured correctly.

    From what you described, it sounds like you are not able to boot your helloword application from BOOT.BIN but are you able to load and run it correctly across the JTAG debug interface?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • denglin12315
    0 denglin12315 over 9 years ago in reply to zedhed

    Hi Kevin,

    I am sorry to took a long time to get back to you.These days we have a long vacation for chinese spring festival.

    Firstly,it works correctly across the JTAG debug interface,but doesn't across SD card only.

    In addition,I have some other questions.As you know,there is one 8GB SD card attached with the picozed SDR2

    development kit,and in the SD card,we can find some image file(linux OS) and run it directly on picozed SDR2,via the hdmi

    interface,we know it is ubuntu and running iio osc application by ADI.

    where can I got source code and cross compile tools to generate these image file? I have already tried to use petalinux

    development my own sofware based on picozed SDR2 and ccfmc,but some device(or function) can't run(such as hdmi,ad9361...etc).

    So,could you give me some suggestions about this?

    Regards,

    -lin.deng

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • denglin12315
    0 denglin12315 over 9 years ago in reply to zedhed

    Hi Kevin,

    I am sorry to took a long time to get back to you.These days we have a long vacation for chinese spring festival.

    Firstly,it works correctly across the JTAG debug interface,but doesn't across SD card only.

    In addition,I have some other questions.As you know,there is one 8GB SD card attached with the picozed SDR2

    development kit,and in the SD card,we can find some image file(linux OS) and run it directly on picozed SDR2,via the hdmi

    interface,we know it is ubuntu and running iio osc application by ADI.

    where can I got source code and cross compile tools to generate these image file? I have already tried to use petalinux

    development my own sofware based on picozed SDR2 and ccfmc,but some device(or function) can't run(such as hdmi,ad9361...etc).

    So,could you give me some suggestions about this?

    Regards,

    -lin.deng