Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development picozed SDR 2x2+vivado 2015.4.2 fbsl can't boot from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1186 views
  • Users 0 members are here
Related

picozed SDR 2x2+vivado 2015.4.2 fbsl can't boot from SD card

denglin12315
denglin12315 over 9 years ago
Hi,everyone
I am using "Picozed SDR 2x2" and "PicoZed SDR FMC Carrier Card AES-PZSDRCC-FMC-G" for my work.
 
But I am facing a problem now.I want to control a led on Carrier Card(connect to zynq pin A8) by the manner of use PS + AXT_GPIO.
 
first, I use vivado create hardware diagram,and export it to SDK,after that ,I use SDK create an application as the template of Memory_Test in SDK and I add my own code to contorl the Led. And then,I use JTAG program FPGA and debug Memory_Test,It all works.
 
After that,I use SDK create an application project as the template of Fbsl in SDK,and using bootgen tools in the SDK create a boot image named boot.bin. Copy boot.bin in a SD card and set boot from SD,the fbsl print some information as follows:
 
--------------------------------------------
Xilinx First Stage Boot Loader 
Release 2015.4  Dec 29 2016-09:33:54
Devcfg driver initialized 
Silicon Version 3.1
Boot mode is SD
SD: rc= 0
SD Init Done 
Flash Base Address: 0xE0100000
Reboot status register: 0x60400000
Multiboot Register: 0x0000C000
Image Start Address: 0x00000000
Partition Header Offset:0x00000C80
Partition Count: 3
Partition Number: 1
Header Dump
Image Word Len: 0x0032D130
Data Word Len: 0x0032D130
Partition Word Len:0x0032D130
Load Addr: 0x00000000
Exec Addr: 0x00000000
Partition Start: 0x000065D0
Partition Attr: 0x00000020
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xFF67242E
Bitstream
In FsblHookBeforeBitstreamDload function 
PCAP:StatusReg = 0x40000A30
PCAP:device ready
PCAP:Clear done
Level Shifter Value = 0xA
Devcfg Status register = 0x40000A30
PCAP:Fabric is Initialized done
PCAP register dump:
PCAP CTRL 0xF8007000: 0x4C00E07F
PCAP LOCK 0xF8007004: 0x0000001A
PCAP CONFIG 0xF8007008: 0x00000508
PCAP ISR 0xF800700C: 0x0802000B
PCAP IMR 0xF8007010: 0xFFFFFFFF
PCAP STATUS 0xF8007014: 0x00003A30
PCAP DMA SRC ADDR 0xF8007018: 0x00100001
PCAP DMA DEST ADDR 0xF800701C: 0xFFFFFFFF
PCAP DMA SRC LEN 0xF8007020: 0x0032D130
PCAP DMA DEST LEN 0xF8007024: 0x0032D130
PCAP ROM SHADOW CTRL 0xF8007028: 0xFFFFFFFF
PCAP MBOOT 0xF800702C: 0x0000C000
PCAP SW ID 0xF8007030: 0x00000000
PCAP UNLOCK 0xF8007034: 0x757BDF0D
PCAP MCTRL 0xF8007080: 0x30800100
...................................................................................................
DMA Done ! 
 
FPGA Done ! 
In FsblHookAfterBitstreamDload function 
Partition Number: 2
Header Dump
Image Word Len: 0x00003003
Data Word Len: 0x00003003
Partition Word Len:0x00003003
Load Addr: 0x00000000
Exec Addr: 0x00000000
Partition Start: 0x00333700
Partition Attr: 0x00000010
Partition Checksum Offset: 0x00000000
Section Count: 0x00000001
Checksum: 0xFFCC3685
Application
Handoff Address: 0x00000000
In FsblHookBeforeHandoff function 
No Execution Address JTAG handof
 
 
 
My tool version is: vavido 2015.4.2.
Thanks.
 
 
 
  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 9 years ago

    Hello denglin12315,

    Linux source code - https://github.com/analogdevicesinc/linux

    Example steps for rebuilding - https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/linux/zynq_2014r2

    Post on rebuilding the HDL project - http://picozed.org/content/how-do-i-rebuild-reference-design-hdl-project

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 9 years ago

    Hello denglin12315,

    Linux source code - https://github.com/analogdevicesinc/linux

    Example steps for rebuilding - https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/linux/zynq_2014r2

    Post on rebuilding the HDL project - http://picozed.org/content/how-do-i-rebuild-reference-design-hdl-project

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • denglin12315
    0 denglin12315 over 9 years ago in reply to mbrown

    Hello Matt,

    Thanks for you replying, it's very helpful!

    -lin.deng