Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development xtmrctr.h file cannot be found
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 363 subscribers
  • Views 4157 views
  • Users 0 members are here
Related

xtmrctr.h file cannot be found

e14 Contributor
e14 Contributor over 12 years ago

I am trying to complete the helloworld tutorial with the imbedded axi_timer and axi_gpio. This is in Chapter 3 of the Zynq ZedBoard Concepts, Tools and Techniques document. After exporting the design to SDK I cannot compile and run the design because the helloworld.c file calls out an include for the xtmrctr.h file.

Where is this file? It does not seem to be included in the zip file where the tutorial came from and I cannot find it on the xilinx web site either.

Any help would be appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Gary, Thanks for the help. That got me farther down the path, but now the compile fails searching for variables such as XPAR_AXI_GPIO_0_DEVICE_ID, XPAR_AXI_TIMER_0_DEVICE_ID, and XPAR_XGPIOPS_NUM_INSTANCES…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Paul, I have seen the issue with XPAR_AXI_GPIO_0_DEVICE_ID and XPAR_AXI_TIMER_0_DEVICE_ID. If you take a look in the xparameters.h file that was generated when the BSP was generated (look in the 'include…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Gary, The xparameters.h file does not have any definitions in it for XPAR_AXI. Are there multiple xparameters.h files that could be copied into my working directory? Does the file depend on the hardware…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Auto Build after a change in the C code is the default but perhaps it is disabled in your configuration. Right click on the Hello_world application under the SDK Project Explorer and perform a 'Clean Project' and, once that is complete, select Hello_world again and perform a 'Build Project'. To verify that you have a new executable you could check the 'properties' of the Hello_world.elf file under the Hello_world project, under 'Debug' to make sure the file was just updated. If the elf file has been updated and the helloworld.c includes the updated application code you should be able to launch the new application as directed.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Gary,

    Thanks for the help. That got me farther down the path, but now the compile fails searching for variables such as XPAR_AXI_GPIO_0_DEVICE_ID, XPAR_AXI_TIMER_0_DEVICE_ID,  and XPAR_XGPIOPS_NUM_INSTANCES.

    Where are these variables supposed to be picked up or defined? I think that I have the hardware defined correctly inside the chip but these are not found.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Paul,

     

    I have seen the issue with  XPAR_AXI_GPIO_0_DEVICE_ID and XPAR_AXI_TIMER_0_DEVICE_ID.  If you take a look in the xparameters.h file that was generated when the BSP was generated (look in the 'include' directory under Hello_world_bsp) you should see that the definitions matching the hardware are  XPAR_AXI_GPIO_1_DEVICE_ID and XPAR_AXI_TIMER_1_DEVICE_ID. You will need to change the definitions in the application code to match the hardware definitions. I think this is due to the current version of the Xilinx tools enumerating hardware instances differently than the version the sample application code was tested with, so the definitions generated by your hardware are slightly different. I have not seen an error with the XPAR_XGPIOPS_NUM_INSTANCES, so I am not sure what your are seeing. In any case, you can always refer to the xparameters.h file for defintions that match your exported hardware. 

     

    -Gary

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Gary,

    The xparameters.h file does not have any definitions in it for XPAR_AXI. Are there multiple xparameters.h files that could be copied into my working directory? Does the file depend on the hardware instantiated in the design? I am running with Vivado 2013.3.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Gary,

    The xparameters.h file does not have any definitions in it for XPAR_AXI. Are there multiple xparameters.h files that could be copied into my working directory? Does the file depend on the hardware instantiated in the design? I am running with Vivado 2013.3.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Xparameters.h is generated based on the hardware instantiated in your design. You could check the 'system.xml' and 'system.mss' files in SDK to see if your design includes the axi_timer and axi_gpio modules.

     

    The current CTT was designed for Vivado 2013.2 and may not work with Vivado 2013.3 without some modifications. As an example: in Vivado 2013.2 when you selected the target board for your project, as you do in the CTT section 2.1.1, the board presets were automatically applied to the project. This was reflected in section 2.1.1 step 7 where it had you click the 'Presets' button and select the ZedBoard Development Board Template' to see the option but then had you 'Cancel' and not apply the presets. In Vivado 2013.3 you would need to apply the presets in step 7 as the board presets are not automatically applied earlier when you selected the target board.

     

    I have not tried to run the CTT through using Vivado 2013.3 yet so I don't know if there will be other issues. If the axi_timer and axi_gpio modules are not reflected in the system.xml and system.mss files in SDK you will need to go back to the Vivado section of the exercise and complete the hardware design first.

     

    -Gary

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    The axi_gpio_0 and axi_timer_0 are shown in the system.xml file under the IP blocks present in the design section. They do not show up in the system.mss file. When I generate the hdl wrapper, do I need to do the step of generate output files first?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    If the axi_gpio and axi_timer modules appear in the system.xml file, which is generated by the Vivado tool and exported to the SDK, that seems to indicate that they are in your hardware design. If the drivers for axi_gpio and axi_timer are not listed in the system.mss under 'Peripheral Drivers' then that implies that the bsp you are using has not be updated or generated to match the latest hardware, as they are generated when the bsp is built. If you have more than one bsp in your project make sure that your application project is referencing the correct one. If you only have one bsp ( Hello_world_bsp as expected) you may need to perform a clean and rebuild of the bsp to make sure it picks up the latest hardware. You can also check the bsp settings and make sure that it is referencing the correct hardware specification under the 'Target Hardware' section.

     

    -Gary