Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development SDK can't program FPGA on MiniZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 650 views
  • Users 0 members are here
Related

SDK can't program FPGA on MiniZed

pgh
pgh over 9 years ago

Hello,

I've been going through the MiniZed tutorial, and I'm getting caught on step 02 - the Hello World application. The SDK can't seem to program the Zynq, although I'm able to connect to it via TTL USB (when the boot switch in the F position) and have set the switch to J (JTAG) boot before plugging it in.

My OS is Ubuntu 16.04.3 LTS, and the SDK is version 17.1.


Below is a screenshot of the issue: https://i.imgur.com/fGSzrGu.png

image

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello poh2017,

    I would just like to verify a few things.

    Did you generated a standalone BSP?

    In the BSP did you changed STDIN and STDOUT to ps7_uart_1?

    You have your MicroUSB connected between J2 and you PC?

    Did you recieve any errors when you imported your hardware platform? Also double check you imported the correct hardware platform.

    Are you able to try this on a Windows 7 PC? That would be worth trying seeing as the tutorials were generated using Windows 7.

    Did you install the Board Definition Files in Vivado? 

     

    From my understanding your issue occurs when your MiniZed is in JTAG boot and you attempt to load the bitstream over the MicroUSB cable connected to J2 via JTAG correct? However, the device is recognizable via a terminal connection.

    I have seen this in the past with MiniZed, this has occured for me when Tera Term was not shutdown or explicitly disconnected when I powered down my MiniZed. This in turn locked up my COM port for an extended period of time.

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello poh2017,

    I would just like to verify a few things.

    Did you generated a standalone BSP?

    In the BSP did you changed STDIN and STDOUT to ps7_uart_1?

    You have your MicroUSB connected between J2 and you PC?

    Did you recieve any errors when you imported your hardware platform? Also double check you imported the correct hardware platform.

    Are you able to try this on a Windows 7 PC? That would be worth trying seeing as the tutorials were generated using Windows 7.

    Did you install the Board Definition Files in Vivado? 

     

    From my understanding your issue occurs when your MiniZed is in JTAG boot and you attempt to load the bitstream over the MicroUSB cable connected to J2 via JTAG correct? However, the device is recognizable via a terminal connection.

    I have seen this in the past with MiniZed, this has occured for me when Tera Term was not shutdown or explicitly disconnected when I powered down my MiniZed. This in turn locked up my COM port for an extended period of time.

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pgh
    0 pgh over 9 years ago in reply to jafoste4

    Yes, I first generated a base hardware platform and then a standalone BSP as shown in the guide. 

    STDIN and STDOUT are both "ps7_uart_1", yes. 

    I have it connected to the computer through J2 only, and there is no disk in USB1.

    I didn't receive any errors, and the hardware platform is definitely the MiniZed.

    This is on a Linux (Ubuntu 16.04) desktop computer. The Board Definition files are installed.

     

    To connect with it for a normal TTL boot, I use the Linux command "screen /dev/ttyUSB1 115200" and get the petalinux root login as expected. The issue seems to be with the SDK's internal terminal program.