Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Efficient way to debug AMP configuration?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 443 views
  • Users 0 members are here
Related

Efficient way to debug AMP configuration?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I am looking for an efficient way to debug an AMP configuration on a ZedBoard. In my configuration core 0 runs a Linux kernel, which then starts the a bare-metal application on the second core via remoteproc/rpmsg.

Now I can connect to just the second core by invoking the command "connect arm hw -debugdevice cpunr 2" in XMD. Then I can also step through the instructions, but I am missing essentially two features:

1. Set a breakpoint to the start of the program and then step through it. The way I do it, I end up in the middle of the program, because I can only connect to the second core once Linux has started the bare-metal application.

2. I would love to have a disassembly rather than just the plain OP-code. A dream would be to be able to debug the bare-metal application graphically directly from XSDK.

Do you think on or even two of my points are realizable?

Thanks,
Sven

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Have you looked at the debugging section near the end of XAPP1078?

     

    http://www.xilinx.com/support/documentation/application_notes/xapp1078-amp-linux-bare-metal.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Have you looked at the debugging section near the end of XAPP1078?

     

    http://www.xilinx.com/support/documentation/application_notes/xapp1078-amp-linux-bare-metal.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Gary,

    thanks for your reply. Now I could get it working. To overcome my first problem, I place an infinite loop at the position I want to stop to connect the debugger:

    volatile int x=1; while(x);

    I then just change the value of x in the debugger.