Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development linker script errors
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 477 views
  • Users 0 members are here
Related

linker script errors

e14 Contributor
e14 Contributor over 12 years ago

Working in Vivado SDK 2014.2, MicroZed z7010 board:

I've been working on a program that collects data from a device off-board, and writes the data to a SD card.  This began as a bare-metal application, which I was able to develop, compile, and test successfully.

Now I am trying to adapt the program to run in the Zynq Linux environment.  I created a new Linux Application Project and copied my source files into it.  I had to change all my references from xil_print to standard print, but otherwise the code seems entirely portable.

However, I have a recurring build error that I cannot figure out how to fix:

error: required section '.got' not found in the linker script
final link failed: Invalid operation
collect2.exe: error: ld returned 1 exit status
make: *** [hyddrate_comms_linux.elf] Error 1

I've found similar errors to this in the forums, but none of the advise has helped so far:
-checked that .got is actually in the linker source
-cleaned out redundant Software Platform Inferred Flags
-reselected the BSP
-confirmed assembler is arm-xilinx-linux-gnueabi-gcc
-confirmed compiler is arm-xilinx-linux-gnueabi-gcc
-confirmed linker is arm-xilinx-linux-gnueabi-gcc

I've refreshed and cleaned the project after each step as well.

Does anyone have more thoughts on what the issue might be?  I am willing to post the source and full console log if that might be useful.

-Adam

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Adam,

      This seems like there might be a problem with the way you converted the project from standalone to a Linux application.  I just tried creating a standalone "helloworld" application project, then an empty Linux application project, and I copied the helloworld source file into it.  Once I removed the platform dependencies from standalone, and converted the "print" statement to "printf", it built fine.  I can generate a link map at this point, by opening the build settings, and adding the following to the Miscellaneous linker options:

    -Wl,-Map=myMap.txt

    This generates the object map in the Debug folder, and when I opened it I could see that indeed the .got section was correctly generated.  If you give this a try and confirm for yourself that the procedure works, it might lead you to a difference in the steps used to port your real application code.

    Ron