Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Problems with fpu commands like sqrt atan
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 463 views
  • Users 0 members are here
Related

Problems with fpu commands like sqrt atan

e14 Contributor
e14 Contributor over 14 years ago

Trying to compile an linux demo project with using sqrt and other math functions including of math.h results in compiler errors. is there no support or what option for compiler is needed?

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 14 years ago

    Hi sbuechele,

    I used 14.2 SDK to put together a quick application to test this out.

    #include <math.h>
    #include <stdio.h>

    int main()
    {
    tdouble angle = 60;
    tdouble square_number = 64;
    tdouble result = 0;

    t/* Calculate the tangent of an angle. */
    tresult = tan(angle);

    tprintf("The tangent of angle %f is %f
    ", angle, result);

    t/* Calculate the square root of a square number. */
    tresult = sqrt(square_number);

        printf("The square root of %f is %f
    ", square_number, result);

        return 0;
    }

    Sure enough, when I go to build I get the error message: "undefined reference to `sqrt'"

    I did a 'man sqrt' and realized my error right away.  The manual for these math functions show that this code must be linked against the math library by adding the '-lm' flag to your build command.

    To do this in SDK, right click on your application project and select the C/C++ Build Settings option.  Then click on the Tool Settings tab and locate the ARM Linux gcc linker-->Libraries pane and add the 'm' library.

    Not only did the application build, but I was able to run it on ZedBoard also:

    zynq> ./math_application.elf
    The tangent of angle 60.000000 is 0.320040
    The square root of 64.000000 is 8.000000

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    thank you