Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development read only rootfs on microsd
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 638 views
  • Users 0 members are here
Related

read only rootfs on microsd

metinburak_
metinburak_ over 11 years ago

Hi,

I want to make the root file system on zedboard read only. Has anybody done this? Any thoughts?

I am making it from fstab but that doesn't make the rootfs readonly; I can even make directories to / folder.

Btw, of course I am using ext4 for rootfs and linaro distro.

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi metinburak_,

    In the interests of helping other forum members, and to show a little respect for the time of those that might be working to answer your post, please post a follow up response with a link to the answer if you have received a response or a solution on another forum. You might be courteous enough to post a link on the other forum if you get a solution here as well.

    http://forums.xilinx.com/t5/Embedded-Linux/read-only-rootfs/td-p/645209

    Have you tried setting the write protect tab of the SD card that is plugged into slot J12?

    I remember when we were bringing up MicroZed for the first time, the Linux kernel we were using at the time would not boot because it could not mount the SD card in read/write mode.  The cause of this was the first hardware configuration we had did not have the SD card WP signal connected to a MIO pin.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • metinburak_
    0 metinburak_ over 11 years ago

    Hi Kevin

    Sure, I will do this if I get a response from other forums.
    http://stackoverflow.com/questions/31702782/read-only-rootfs-zynq-zedboard

    Can we make this via the WP pin from PL side at runtime?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    ZedBoard uses a full-size SD Card, not microSD. Full-size SD Cards have a WP connection between the card, the connector, and onto the ZedBoard, which is connected to net name SD-WP, which is connected to MIO46. As long as you have properly connected WP in the SDIO controller in the PS and set the WP switch on the SD Card, then the driver should prevent the card from being written.

     

    Bryan