Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development I2C audio codec
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 362 subscribers
  • Views 226 views
  • Users 0 members are here
Related

I2C audio codec

e14 Contributor
e14 Contributor over 12 years ago

Hello

I'm trying to generate a sinewave with 1khz of frequency and send it to output audio line.

DAC is configurated to 48 kHz, so the sample rate i am using is 48kHz. I create LUT with that samples and i'm sending the samples to the output line.

I already tried sending from my PC to line in a 1khz sine wave and then directing it to line out and all went good. The values are more or less similar to the samples that I have but when i try to generate the sine samples in a C program and then output them to line out the sound is completely wrong.

The function that i used is this one:






void audio_stream(){
//u32 in_left, in_right;
int i,j=0;
int size=96000; // 96000 amostras para ter 2 segundos de som
u32 audio,aux[48];//,audio2;

printf("Inicializando a LUT
");
for(i=0;i<48;i++){
aux[i]=((sin(((2*M_PI)/(48))*(i))*pow(2,24))+pow(2,24)-1)/2;
//printf("Iteracao= %d AUX= %d
",i,aux[i]);
}
printf("--------------------
");
printf("LUT Criada!
");


while (!XUartPs_IsReceiveData(UART_BASEADDR)){
// Read audio input from codec
//in_left = Xil_In32(I2S_DATA_RX_L_REG);
//in_right = Xil_In32(I2S_DATA_RX_R_REG);

// Write audio output to codec
audio=(u32)aux[j%48];
Xil_Out32(I2S_DATA_TX_L_REG, audio);
j++;
//2880000
if(j>=size){
//printf("j= %d
",j);
menu();

}
//printf("audio= %lx aux= %d
",audio,aux);
//printf("right= %d",in_right);
//Xil_Out32(I2S_DATA_TX_L_REG, audio);
//Xil_Out32(I2S_DATA_TX_R_REG, (u32)audio);//
}


/* If input from the terminal is 'q', then return to menu.
* Else, continue streaming. */
if(XUartPs_ReadReg(UART_BASEADDR, XUARTPS_FIFO_OFFSET) == 'q') menu();
else audio_stream();

} // audio_stream()








What i'm doing wrong? Is this method impossible to implement? Or i'm forgoting something?

Thanks for the help
Joao

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    I don't know the answer to your question, but you may also get some ADAU1761 help on the Analog Devices forums at http://wiki.analog.com.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    I don't know the answer to your question, but you may also get some ADAU1761 help on the Analog Devices forums at http://wiki.analog.com.

    Bryan