Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AMP Connect HW to ARM1 Bare-Metal with Linux on ARM0
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 470 views
  • Users 0 members are here
Related

AMP Connect HW to ARM1 Bare-Metal with Linux on ARM0

e14 Contributor
e14 Contributor over 13 years ago

How do I tell Linux which devices are available to ARM1 running a bare metal application?

I've built and run Xapp1078 successfully. I've added UART0 through EMIO to the HW. I built a new device-tree for Linux. The Linux app rwmem.elf can access the UART0 memory at 0xE0000000.

When running the bare-metal app with the debugger I cannot access UART0 at 0xE0000000. I can however access UART1 at 0xE0001000. I can write to the Linux console from ARM1.

I have successfully accessed UART0 from a standalone app.

I need to configure the system to access UART0 and other HW from ARM1 (i.e. SPI0, SPI1, etc.). This seems like it should be simple to do but I've not been very successful.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The XSDK libraries from ISE 14.6 appear to have solved the problem. I have successfully written to UART0 and the LEDs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The XSDK libraries from ISE 14.6 appear to have solved the problem. I have successfully written to UART0 and the LEDs.