Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development minized - [Place 30-58] IO placement is infeasible
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 2712 views
  • Users 0 members are here
Related

minized - [Place 30-58] IO placement is infeasible

andycap
andycap over 9 years ago

Hi Guys,

 

I have the 2017.2 Vivado project from github, I have built this and generated a petalinux buils which boots on the minized.

 

My next task was to add some IP, as an initial simple test I have just changed the axi_gpio_1 to dual mode and added an output mapped to M9, I have the following set in the constraints file:

set_property PACKAGE_PIN M9 [get_ports pl_gpio_test]

set_property IOSTANDARD LVCMOS33 [get_ports pl_gpio_test]
 
 
 
When I generate in vivado I get the following error:
 

[Place 30-58] IO placement is infeasible. Number of unplaced terminals (1) is greater than number of available sites (0).

The following Groups of I/O terminals have not sufficient capacity:
 IO Group: 0 with : SioStd: LVCMOS18   VCCO = 1.8 Termination: 0  TermDir:  Out  RangeId: 1 Drv: 12  has only 0 sites available on device, but needs 1 sites.
        Term: pl_gpio_test_tri_o[0]
 
 
If I look at the I/O bank properties in vivado  the output is correct on bank 35, pin M9, LVCMOS33, output.
 
I'm a bit stumped by this, I have been using a zybo board before and have not seen this error before and there doesn't seem to be much about it on the internet.
 
Anyone got any ideas?
 
Cheers
 
Andy
 
 
 
 
  • Sign in to reply
  • Cancel
  • andycap
    0 andycap over 9 years ago

    Ok, fixed it. I changed the constraints to:

     

    set_property PACKAGE_PIN M9 [get_ports pl_gpio_test_tri_o]

    set_property IOSTANDARD LVCMOS33 [get_ports pl_gpio_test_tri_o]

     
     
    Why am I having to add a _tri_o to the end of the port name in this project?
     
    Cheers
     
    Andy
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 9 years ago

    Ok, fixed it. I changed the constraints to:

     

    set_property PACKAGE_PIN M9 [get_ports pl_gpio_test_tri_o]

    set_property IOSTANDARD LVCMOS33 [get_ports pl_gpio_test_tri_o]

     
     
    Why am I having to add a _tri_o to the end of the port name in this project?
     
    Cheers
     
    Andy
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi Andy,

    Vivado appends your signal name with "tri_i" or "tri_io" or "tri_o" depending on the IO type when the Create HDL wrapper script generates the wrapper.  The appended name depends on whether the signal is defined as input only, input/output, or output only respectively within your GPIO block.

    For information on tracking down IO placement errors, see the discussion on this Xilinx thread:

    https://forums.xilinx.com/t5/Implementation/IO-Standard-default-when-XDC-clearly-defines-location-and-io/td-p/781856

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • andycap
    0 andycap over 9 years ago

    Hi Kevin,

     

    Thanks very much for the info and the link, I will read it carefully,

     

    All the best

    Andy