Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Starting a application with u-boot on Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 365 subscribers
  • Views 1658 views
  • Users 0 members are here
Related

Starting a application with u-boot on Microzed

e14 Contributor
e14 Contributor over 10 years ago

Hi,
I'm trying to start a RTEMS application on the Microzed Board with u-boot. The .bin file is located on the SD card. I try it the following way:
  1. fatload mmc 0 0x100000 ticker.bin
  2. go 100000
Than it freezes with:
## Starting application at 0x00100000 ...

When I try to bootm the image of ticker.bin with:
  1. fatload mmc 0 100000 ticker.img
  2. bootm 100000
it freezes with:
## Booting kernel from Legacy Image at 00100000 ...                                          
   Image Name:   RTEMS Application                                                           
   Image Type:   ARM RTEMS Kernel Image (uncompressed)                                       
   Data Size:    1039080 Bytes = 1014.7 KiB                                                  
   Load Address: 30000100                                                                    
   Entry Point:  30000100                                                                    
   Verifying Checksum ... OK                                                                 
   Loading Kernel Image ... OK                                                               
OK                                                                                           
## Transferring control to RTEMS (at address 30000100) ...

I use the U-Boot 2013.01-dirty version of u-boot. RTEMS is a bare metal application

Regards

  • Sign in to reply
  • Cancel
Parents
  • arturete
    0 arturete over 9 years ago

    All the setup was ok.

    I created the FSBL.elf and the BOOT.bin with the SDK, as you indicated me in the last comment, instead of the terminal.

    It started working when I used the hello.ralf file instead of the hello.exe, and I renamed it to hello.elf.

    I putted those files plus the .bit in the SD and the application is launched and works.

    As you told me for the next issues I will use the Digilent forum.


    THANKS,
    Arturete.



     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • arturete
    0 arturete over 9 years ago

    All the setup was ok.

    I created the FSBL.elf and the BOOT.bin with the SDK, as you indicated me in the last comment, instead of the terminal.

    It started working when I used the hello.ralf file instead of the hello.exe, and I renamed it to hello.elf.

    I putted those files plus the .bit in the SD and the application is launched and works.

    As you told me for the next issues I will use the Digilent forum.


    THANKS,
    Arturete.



     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer